Hi,
We recently received our custom board with the i.MX6ULL processor.
It's fairly similar to the EVK, however, one ethernet PHY has been omitted and an eMMC is used instead of the SD card.
Unfortunately, I am having some trouble bringing up the board.
I tried using uuu with the provided sample images.
Host terminal:
sudo ./uuu uuu.auto-imx6ull14x14evk
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-15-gd1c466c
Success 0 Failure 0
1:15 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx6ull14x14evk_emmc.imx
Board terminal:
U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:49:03 +0000)
CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 51C
Reset cause: POR
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment[*]-Video Link 0 (480 x 272)
.[0] lcdif@21c8000, video
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net: Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000
It repeats this loop every couple seconds.
Does this mean that not finding the PHY is blocking the next step ?
Any help is appreciated !
解決済! 解決策の投稿を見る。
Thanks for your reply!
The PHY was omitted in hardware.
The reason u-boot was blocking, was not that the PHY was missing, but that it had the wrong address.
Thanks for your reply!
The PHY was omitted in hardware.
The reason u-boot was blocking, was not that the PHY was missing, but that it had the wrong address.
how did you omit the phy? did you change the dts file of uboot?