Hello,
Basically it is possible to arrange a chain of several devices, supporting JTAG Boundary Scan,
in order to test all devices in the chain. If the DDR3 and eMMC do not support such feature,
only i.MX6UL can be tested via Boundary Scan JTAG. Note, i.MX6 JTAG_MOD signal should be
pulled up for it.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!