Boundary Scan for MCIMX6Q5EYM12AD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boundary Scan for MCIMX6Q5EYM12AD

1,086 Views
bhagathsingh
Contributor I

Hello,

I am trying to run a boundary scan on MCIMX6Q5EYM12AD using J-link from IAR Systems and TopJTAG Probe software tool. Below is the board settings which I have used

TEST_MODE is Low;

JTAG_MOD is High;

POR_B is High;

BOOT_MODE[1:0] is [1:0].

 

When I try to detect the JTAG devices connected, it shows No JTAG Chain Detected. Kindly help me resolve this issue.

Thanks

Bhagath

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

907 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bhagath

one can check jtag signal levels for both processor and JTAG device,

check clocks and power supplies described in i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

[SOLVED] How to do a simple JTAG (boundary) scan? - J-Link/Flasher related - SEGGER - Forum 

Isues with usage TopJTAG Probe software can be posted on support forum for that software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------