Boundary Scan bidirectional pins imx6 MCIMX6U5DVM10AB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boundary Scan bidirectional pins imx6 MCIMX6U5DVM10AB

2,816 Views
julianmp
Contributor II

I can't check the inputs with boundary scan . I 'm able to set output pins and Z state but It's imposible for me to check the input. For example, in I2C  I manage to make all the trace but I'm not able to check the respond ACK . Even though, I know the respond It's OK because I'm using an oscyloscope to check it. I don't know how I have to set the bsr register to check the input, I paste piece of my svf script( In the first row the 8 it's the z state to allow the I2C slave respond but I don't know how to check them.  Can I have some help, please?

SDR 648 TDI (000000000000000000100800000000000000000000000000000000000000000000000000000000000000000000000004000000000000000000000000000000000000000000000000000000004000000144)
TDO (000000000000000000000400000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000)
MASK (000000000000000000000400000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000);

Labels (1)
6 Replies

2,620 Views
julianmp
Contributor II

   Hi Yuri, I have those configuration but the input still doesn't work. For example, If I try to check the i2c ACK I can't figured out If it is an ACK or a NACK becuse the input appears not to work. I setup the control pin to 1 and the output pin to 0 but It only makes a Z state but I'm not able to check the input. Do you have any idea about this problem?

0 Kudos
Reply

2,620 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please provide detailed description (log) of all activities, used to detect the I2C ACK,

starting from JTAG reset.

Regards,

Yuri.

0 Kudos
Reply

2,620 Views
julianmp
Contributor II

Thanks for the support, finally I managed to run it. I had weak soldering in the soc pins.

2,620 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Generally SAMPLE/PRELOAD Instruction is used "to obtain a snapshot of

system data and control signals". Please look at Chapter 56 [System JTAG

Controller (SJC)] of i.MX 6Solo/6DualLite Reference Manual,Rev. 2, 04/2015.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,620 Views
julianmp
Contributor II

Hi Yuri, I made the things that you have told me.

SAMPLE/PRELOAD Instruction

dr instruction to get the tdo values and it's value 0x00000...

So I think something is wrong with the input maybe the bsdl or something else

Thanks for the help

0 Kudos
Reply

2,620 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please check SATA and PCIe power supply pins, which are needed to be powered before boundary scan mode. Please look at Table 2-21 (Recommended connections for unused analog interfaces) of the Hardware Development
Guide.

http://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf 

For Boundary Scan JTAG_MOD should be high.

Please look at Table 2-5 (JTAG recommendations) of the Hardware Development Guide.

Also, please pay attention on COMPLIANCE_PATTERNS of the BSDL file.
attribute COMPLIANCE_PATTERNS of MX6Q: entity is
"(TEST_MODE, JTAG_MOD, POR_B) (011)";

Check if :
TEST_MODE is LOW ;
JTAG_MOD is HIGH ;
POR_B is HIGH.

Regards,

Yuri.

0 Kudos
Reply