Booting linux from NAND Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting linux from NAND Flash

2,247 次查看
cnguyenterasci
Contributor I

When I boot my device from NAND flash, everything goes ok but it just stops booting at "Waiting for root device /dev/mmcblk0p3..."

标签 (2)
0 项奖励
回复
5 回复数

1,916 次查看
cnguyenterasci
Contributor I

I ran the MFG Tool and loaded linux on the NAND flash.  I h ave the jumpers set to be booting from NAND flash as well. 

0 项奖励
回复

1,916 次查看
jimmychan
NXP TechSupport
NXP TechSupport

When the board booting up, there is a "Kernel Command line". Please check the root filesystem location. it should be something like "root=/dev/xxxxxxxx". For NAND, should be like this root=/dev/mtdblock1.

1,916 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Is your filesystem store in the SD Card? according to your message, it is looking for the rootfs from the SD Card (mmcblk0) partition 3. Please double check the bootargs in uboot used is correct or not.

0 项奖励
回复

1,916 次查看
sinanakman
Senior Contributor III

Calvin, which device, which board is this ?

0 项奖励
回复

1,916 次查看
cnguyenterasci
Contributor I

i.Mx233.  I have an EVK board as well as a board I designed and I get the same thing on both boards.

0 项奖励
回复