Booting issue in Android Lollipop BSP in I.MX sabre6q board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting issue in Android Lollipop BSP in I.MX sabre6q board

ソリューションへジャンプ
13,527件の閲覧回数
arunsrk91
Contributor II

Hi All,

 

I am new to building and setting i.mx android bsp image. I have downloaded the i.MX6 Android L5.0.0_1.0.0 BSP Documentation

cd ~/myandroid/

sudo chmod +x ./device/fsl/common/tools/fsl-sdcard-partition.sh

sudo ./device/fsl/common/tools/fsl-sdcard-partition.sh -f imx6q /dev/sdc

 

The partition and flashing is success and booting is starting but am getting the following error. Please find the below log and kindly guide me in solving the issue.

 

U-Boot 2014.04-08648-g9d7bf9b (Oct 09 2015 - 19:34:25)

 

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 24 C, calibration data: 0x5584a97d

Reset cause: POR

Board: MX6-Sabreauto revA

I2C:   ready

DRAM:  2 GiB

NAND:  0 MiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

 

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=11

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:1

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

booti mmc1

kernel   @ 14008000 (6819472)

ramdisk  @ 15000000 (725570)

fdt      @ 14f00000 (50535)

kernel cmdline:

        use boot.img command line:

        console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M8

   Using Device Tree in place at 14f00000, end 14f0f566

 

Starting kernel ...

 

Booting Linux on physical CPU 0x0

Initializing cgroup subsys cpu

Initializing cgroup subsys cpuacct

Linux version 3.10.53-88204-g4f0dd92 (root@aricent-OptiPlex-390) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 SMP PREEM5

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Automotive Board

cma: CMA: reserved 384 MiB at 5e000000

Memory policy: ECC disabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @82008000 s9728 r8192 d14848 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 520768

Kernel command line: console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off8

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)

Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)

Memory: 1983MB 64MB = 2047MB total

Memory: 1666872k/1666872k available, 430280k reserved, 424960K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xe6800000 - 0xff000000   ( 392 MB)

    lowmem  : 0x80000000 - 0xe6000000   (1632 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80e7a48c   (14794 kB)

      .init : 0x80e7b000 - 0x80ed0600   ( 342 kB)

      .data : 0x80ed2000 - 0x80f56000   ( 528 kB)

       .bss : 0x80f56000 - 0x80feacf8   ( 596 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.2

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux:  Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x807e23e8 - 0x807e2440

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1100 mV

vdd3p0: 2625 <--> 3400 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2400 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

cs42888_supply: 3300 mV

vio1: 3300 mV

vio2: 3300 mV

vd: 3300 mV

va: 5000 mV

platform usb_h1_vbus.33: Driver reg-fixed-voltage requests probe deferral

platform usb_otg_vbus.34: Driver reg-fixed-voltage requests probe deferral

3P3V: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

pureg-dummy: no parameters

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 5, 131072 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP: reno registered

UDP hash table entries: 1024 (order: 3, 32768 bytes)

UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 708K (85000000 - 850b1000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

mxc_epit: probe of 20d0000.epit failed with error -22

mxc_epit: probe of 20d4000.epit failed with error -22

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

console [pstore-1] enabled

ramoops: attached 0x100000@0x8bf00000, ecc: 0/0

mxc_ramoops device success loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

audit: initializing netlink socket (disabled)

type=2000 audit(0.490:1): initialized

bounce pool size: 64 pages

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/W DEBUG].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 3194

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

MIPI DSI driver module loaded

mxc_sdc_fb fb.23: registered mxc display driver ldb

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb fb.24: Can't get fb option for mxcfb1!

mxc_sdc_fb fb.25: Can't get fb option for mxcfb2!

mxc_sdc_fb fb.26: Can't get fb option for mxcfb3!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 0-0008: Full lay: 1, Metal lay: 1

pfuze100-regulator 0-0008: FAB: 0, FIN: 0

pfuze100-regulator 0-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1375 mV

SW1C: 300 <--> 1875 mV at 1375 mV

SW2: 800 <--> 3300 mV at 3000 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 1975 mV at 1800 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 800 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 1800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 2500 mV

VGEN6: 1800 <--> 3300 mV at 2800 mV

Serial: IMX driver

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

console [ttymxc3] enabled

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

si476x-core 0-0063: Using default platform data.

si476x-core 0-0063: No IRQ number specified, will use polling

si476x-core 0-0063: Error while sending command 0x11

si476x-core 0-0063: The device in inconsistent power state

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

CAN device driver interface

flexcan 2094000.can: device registered (reg_base=e69e8000, irq=143)

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

PPP generic driver version 2.4.2

PPP BSD Compression module registered

PPP Deflate Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

usbcore: registered new interface driver asix

usbcore: registered new interface driver ax88179_178a

usbcore: registered new interface driver cdc_ether

usbcore: registered new interface driver net1080

usbcore: registered new interface driver cdc_subset

usbcore: registered new interface driver zaurus

usbcore: registered new interface driver cdc_ncm

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver option

usbserial: USB Serial support registered for GSM modem (1-port)

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

platform 2184000.usb: Driver imx_usb requests probe deferral

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

platform 2184200.usb: Driver imx_usb requests probe deferral

mousedev: PS/2 mouse device common for all mice

usbcore: registered new interface driver xpad

usbcore: registered new interface driver usb_acecad

usbcore: registered new interface driver aiptek

usbcore: registered new interface driver gtco

usbcore: registered new interface driver hanwang

usbcore: registered new interface driver kbtab

usbcore: registered new interface driver wacom

egalax_ts 0-0004: Failed to wake up, disable suspend,otherwise it can not wake up

egalax_ts 0-0004: Failed to read firmware version

egalax_ts: probe of 0-0004 failed with error -5

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

DBG sensor data is at 80fc48a0

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.41: V4L2 device registered as video17

usbcore: registered new interface driver uvcvideo

USB Video Class driver (1.1.1)

gspca_main: v2.14.0 registered

mag3110 1-000e: check mag3110 chip ID

mag3110 1-000e: read chip ID 0xfffffffb is not equal to 0xc4!

mag3110: probe of 1-000e failed with error -22

mma8x5x 1-001c: read chip ID 0xfffffffb is not equal to 0x1a,0x2a,0x3a,0x4a,0x5a!

mma8x5x: probe of 1-001c failed with error -22

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

device-mapper: uevent: version 1.0.3

device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

usbcore: registered new interface driver btusb

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc2: no vmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

Galcore version 5.0.11.25762

mmc2: new high speed SDHC card at address e624

mmcblk2: mmc2:e624 SU08G 7.40 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk2: p4 size 13352010 extends beyond EOD, truncated

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ashmem: initialized

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

cs42xx8 0-0048: failed to get device ID, ret = -5

cs42xx8: probe of 0-0048 failed with error -5

fsl-hdmi-dai hdmi_audio.17: failed to probe. Load HDMI-video first.

fsl-hdmi-dai: probe of hdmi_audio.17 failed with error -12

imx-cs42888 sound-cs42888.36: failed to find codec platform device

imx-cs42888: probe of sound-cs42888.36 failed with error -22

imx-spdif sound-spdif.39:  dir-hifi <-> 2004000.spdif mapping ok

imx-audio-hdmi sound-hdmi.38: initialize HDMI-audio failed. load HDMI-video first!

imx-tuner-si476x sound-fm.37: failed to find FM platform device

imx-tuner-si476x: probe of sound-fm.37 failed with error -22

NET: Registered protocol family 26

u32 classifier

    Actions configured

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (16384 buckets, 65536 max)

ctnetlink v0.93: registering with nfnetlink.

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

xt_time: kernel timezone is -0000

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

mip6: Mobile IPv6

ip6_tables: (C) 2000-2006 Netfilter Core Team

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN2: disabling

SWBST: disabling

SW4: disabling

regulator-dummy: disabling

imx mcc test is registered.

usb_h1_vbus: 5000 mV

usb_otg_vbus: 5000 mV

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: EHCI Host Controller

usb usb1: Manufacturer: Linux 3.10.53-88204-g4f0dd92 ehci_hcd

usb usb1: SerialNumber: ci_hdrc.0

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb2: Product: EHCI Host Controller

usb usb2: Manufacturer: Linux 3.10.53-88204-g4f0dd92 ehci_hcd

usb usb2: SerialNumber: ci_hdrc.1

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.20 as /devices/soc0/gpio-keys.20/input/input0

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)

ALSA device list:

  #0: imx-spdif

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

type=1403 audit(1.720:2): policy loaded auid=4294967295 ses=4294967295

type=1404 audit(1.730:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

bio: create slab <bio-1> at 1

device-mapper: verity: data block 0 is corrupted

EXT4-fs (dm-0): unable to read superblock

fs_mgr: __mount(source=/dev/block/dm-0,target=/system,type=ext4)=-1

fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/dm-0 at /system options: barrier=1 error: Invalid argument

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p4): recovery complete

EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk2p6): recovery complete

EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0

init: fs_mgr_mount_all returned an error

init: fs_mgr_mount_all returned unexpected error 255

init: cannot find '/system/bin/logd', disabling 'logd'

init: cannot find '/system/bin/lmkd', disabling 'lmkd'

binder: 140:140 transaction failed 29189, size 0-0

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.product.manufacturer'

init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufacturer'

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'

init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'

android_usb: already disabled

mtp_bind_config

binder: 140:140 transaction failed 29189, size 0-0

binder: 140:140 transaction failed 29189, size 0-0

binder: 140:140 transaction failed 29189, size 0-0

binder: 140:140 transaction failed 29189, size 0-0

binder: 140:140 transaction failed 29189, size 0-0

                                                  

 

 

 

Thanks and Regards,

Arun S

Original Attachment has been moved to: boot-log.txt.zip

ラベル(2)
0 件の賞賛
返信
1 解決策
6,712件の閲覧回数
devarajgs
NXP Employee
NXP Employee

This is specific to Lollipop, when you are trying to build the images for SD card booting.

You need to follow the steps I mentioned.

元の投稿で解決策を見る

0 件の賞賛
返信
24 返答(返信)
1,070件の閲覧回数
arunsrk91
Contributor II

Hi All,

The issue was due to some error in disk partitioning and flashing. I tried the same in an older kernel version and booting was success. But unlike other android BSP, am not able to enter commands from console in lollipop. How to set the U-boot environment variables? How to keep alive the screen through command? Please suggest some solution.

thanks and regards,

Arun S

0 件の賞賛
返信
1,070件の閲覧回数
devarajgs
NXP Employee
NXP Employee

Hi,

The default images that you build works for the eMMC but to boot the image from the SD card, you need to follow the below instructions:

3.4.3 Building Android image for the SD card on the SABRE-SD

Board

The default configuration in the source code package takes internal eMMC as the boot storage. It can be changed to make the

SD card in SD Slot 3 as the boot storage as follows:

remove out/target/product/sabresd_6dq/root directory and boot*.img

remove /out/target/product/sabresd_6dq/recovery directory and recovery*.img

remove /out/target/product/sabresd_6dq/system directory and system*.img

$ make BUILD_TARGET_DEVICE=sd

Follow Section 3.4 to build the images.

For more information please refer to the Android_User_Guide.pdf from the documentation section.

Thanks and Regards,

-Devaraj

0 件の賞賛
返信
1,070件の閲覧回数
arunsrk91
Contributor II

Hi Devaraja,

Thank you for your response. But when i tried the same procedure in another system(Ubuntu 12.04) , everything went well. I am not sure if its some issues with kernel module of my build system.

Thanks and Regards,

Arun S

0 件の賞賛
返信
6,713件の閲覧回数
devarajgs
NXP Employee
NXP Employee

This is specific to Lollipop, when you are trying to build the images for SD card booting.

You need to follow the steps I mentioned.

0 件の賞賛
返信