Booting configuration for SLC Parallel Raw NAND I.MX RT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting configuration for SLC Parallel Raw NAND I.MX RT1170

597件の閲覧回数
TM_MI
Contributor III

Hello,

I am configuring Boot_CFG.

BOOT_CFG1[0] is boot search count of FCB and DBBT.

BOOT_CFG[11] is reserved with default value High-Z but I think it should be pulled Up/Down.

I checked reference manual section about this but still confused about these bits.

Could someone please explain how to configure these two bits?

 

Thanks,

Tarek

0 件の賞賛
返信
1 返信

586件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could someone please explain how to configure these two bits?
-- Regarding SEMC (NAND) boot, the BOOT_CFG[11] doesn't work at all, in another word, it won't affect the boot-up process no matter of the value is.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信