Booting Problem of SABRE i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting Problem of SABRE i.MX6

2,963件の閲覧回数
kahjoolee
Contributor II

Hi,

I'm new to the iMX6 platform and we just bought the SABRE Board for Smart Devices of i.MX6 Quad Core.

Would like to boot the from the SD but nothing was show on the LCD monitor Screen.

When connect to the USB Debug port, below is the log file.

How I can continue to boot from there?

How I can chang the OS from the SD to LINUX base OS?

U-Boot 2009.08 (Apr 29 2013 - 18:01:51)

CPU: Freescale i.MX6 family TO1.5 at 792 MHz
Thermal sensor with ratio = 180
Temperature: 32 C, calibration data 0x5724cc7d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63015 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Found PFUZE100! deviceid=10,revid=21
Net: got MAC address from IIM: 00:04:9f:04:9d:b9
FEC0 [PRIME]
Hit any key to stop autoboot: 0
booti: bad boot image magic
fastboot is in init......flash target is MMC:3
Bad partition index:1 for partition:boot
Bad partition index:2 for partition:recovery
Bad partition index:5 for partition:system
wait usb cable into the connector!


U-Boot 2009.08 (Apr 29 2013 - 18:01:51)

CPU: Freescale i.MX6 family TO1.5 at 792 MHz
Thermal sensor with ratio = 180
Temperature: 35 C, calibration data 0x5724cc7d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63015 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Found PFUZE100! deviceid=10,revid=21
Net: got MAC address from IIM: 00:04:9f:04:9d:b9
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MX6Q SABRESD U-Boot > boot
booti: bad boot image magic
fastboot is in init......flash target is MMC:3
Bad partition index:1 for partition:boot
Bad partition index:2 for partition:recovery
Bad partition index:5 for partition:system
wait usb cable into the connector!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,392件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi KAH

please try latest Demo Images

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_MX6QDLSOLO&appType=license&location=null&Pa... 

for programming use attached Linux Guide sect.4.3 Preparing an

SD/MMC card to boot, sect.4.3.2 Copying the full SD card image

check additional docs

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor

0 件の賞賛
返信

2,392件の閲覧回数
kahjoolee
Contributor II

Hi,

May I know after downlaod the BSP file, which of the file can be use to boot the CPU after extract in the Ubuntu?

Which file that I can used to download the file to the SD Card?

Thanks.

0 件の賞賛
返信

2,392件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi,

It looks like that partitions on your SD card are bad. How you burned image onto SD card?

Michal