Booting IMX51 from SD/MMC(klm8g2fe3b-b001)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting IMX51 from SD/MMC(klm8g2fe3b-b001)

Jump to solution
1,348 Views
Arcatus
Contributor II

Hi All,

I am using IMX51 and  boot it from SD/MMC(klm8g2fe3b-b001) successfully,but someday i make a wrong eboot menu lead to uable to restart and no output in serial console,but  I can burn  burn right image file byAdvanced tookit successfully.why?

Wrong eboot menu configuration that i make,below.

-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item 
-----------------------------------------------------------------------------
[0] IP Address : 0.0.0.0
[1] Set IP Mask : 0.0.0.0
[2] Boot Delay : 3
[3] DHCP : Disabled
[4] Reset to Factory Default Configuration
[5] Select Boot Device : NK from SD/MMC
[6] Set MAC Address : FF-FF-FF-FF-FF-FF
[7] Format OS NAND Region
[8] Format All NAND Regions
[9] Bootloader Shell
[I] KITL Work Mode : Interrupt
[K] KITL Enable Mode : Disable
[P] KITL Passive Mode : Disable
[S] Save Settings
[D] Download Image Now
[L] Launch Existing Flash Resident Image Now
[E] Select Ether Device : FEC
[M] MMC and SD Utilities

Selection: M

-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item 
-----------------------------------------------------------------------------
[A] eMMC 4.3 Boot Partition : Disabled / Not Available
[B] eMMC 4.3 Boot Partition Size : 2048 Kbytes
[S] eSD 2.1 Boot Partition : Disabled / Not Available
[D] eSD 2.1 Boot Partition Size : 0 Kbytes                                     (error chose)
[C] Create File System Partition on SD/MMC Boot Card                      (right chose)
[F] Format All SD/MMC Regions
[R] Return to Main Menu

Right chance is C,but I chose the wrong chance A or Bor Sor D,I can't remeber it.when i chosed it ,the board can't start normally,and a serial port can't print anything,but I can burn burn right image file by Advanced tookit successfully in download mode.why?

Thanks,

Arcatus

Labels (2)
Tags (3)
1 Solution
948 Views
igorpadykov
NXP Employee
NXP Employee

I think you could try to experiment with different eMMC

and find reason what is wrong. If you are using eMMC 4.41

(klm8g2fe3b-b001) which is not supported by i.MX51 (according

to documentation) you can not expect normal operation.

~igor

View solution in original post

0 Kudos
4 Replies
948 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arctic

ATK ToolKit just perform raw writing to SD sectors, it runs without OS and do not use partitions

info. While MFG Tool is small linux image it expect to see SD card among its devices.

To answer your question it is necessary to know what exact manipulations you

did, so it may be recommended just to try reproduce this issue once more time.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

948 Views
Arcatus
Contributor II

hi igorpadykov

Wrong choose lead to be unable to start and serial port can't print any information,how should i do with?

0 Kudos
949 Views
igorpadykov
NXP Employee
NXP Employee

I think you could try to experiment with different eMMC

and find reason what is wrong. If you are using eMMC 4.41

(klm8g2fe3b-b001) which is not supported by i.MX51 (according

to documentation) you can not expect normal operation.

~igor

0 Kudos
948 Views
Arcatus
Contributor II

I will follow your suggestion,and have a try.

thanks,

Arctic

0 Kudos