Hi Gusarambula ,
Thanks for your reply .
i had downloaded binaries from below link
IMX6_M6.0.1_2.1.0_ANDROID_DEMO_iMX7D_BSP
Now , i have done partition as before (PFA) but now i am booting the board with uboot-imx7d.imx in place of uboot-imx7d.bin and dd the images without seek parameter except in uboot-imx7d.imx. and i am getting the logs . please find the log as an attachment.(PFA) , but i am not getting full logs of android .
So Now , as suggested by you , i am going to make the partition according to mentioned in the android user guide
http://support.keith-koep.com/service/lib/exe/fetch.php/service/linux/android_user_guide.pdf
But , if you see on page 11 of the doc , i have some confusion . please answer .
1> i will not have to reserve separate partition for u-boot as i did before and will flash/write uboot-imx7d.img into /dev/sdd partition. right ?
2>on the page 11 , if you see , for boot-imx7d.img partition , file system type for boot partition is boot.img format , so for this partition , what type of file system should i keep , because there is no option called boot.img format while making partition. should i make it FAT32 ? or what ?
3> Also , using gparted , i am making partitions ; But gparted do not let me to make many logical partitions as mentioned in the document.so how can i make such partition
as i do not have the script that make such partition .
one more thing , it will be very nice , if you explain in a line or two regarding the problem , we were having due to "seek " parameter in the dd command . why seek causing a problem ? that will help me to understand the problem better.
Thanks and Regards,
Mehul