Boot speed of the imx.8plus. Why is the kernel slow to initialize emmc?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot speed of the imx.8plus. Why is the kernel slow to initialize emmc?

926 Views
chen-wust
Contributor II

To make the processor boot faster, I changed the emmc read mode from the default mode(HS 52M) to HS200(200M).I achieved this by modifying the device tree of uboot:Add the following properties.

mmc-hs200-1_8v;

In uboot, emmc read speed increased from 30M/S to 60M/S.

However, this affects the kernel boot speed, and the kernel initializing emmc is one second slower, making the overall boot speed slower.

May I ask what causes this problem? I really hope to get your help and reply.

May I ask what causes this problem? Can you give some suggestions to solve this problem? I really hope to get your help and reply

0 Kudos
Reply
1 Reply

912 Views
chen-wust
Contributor II

uboot emmc dts:

&usdhc2 {
	pinctrl-names = "default", "state_100mhz", "state_200mhz";
	pinctrl-0 = <&pinctrl_usdhc2>;
	pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
	pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
	vmmc-supply = <&reg_usdhc2_vmmc>;
	bus-width = <4>;
broken-cd; status = "okay"; }; &usdhc3 { pinctrl-names = "default", "state_100mhz", "state_200mhz"; pinctrl-0 = <&pinctrl_usdhc3>,<$pinctrl_usdhc3_gpio>; pinctrl-1 = <&pinctrl_usdhc3_100mhz>,<$pinctrl_usdhc3_gpio>; pinctrl-2 = <&pinctrl_usdhc3_200mhz>,<$pinctrl_usdhc3_gpio>; bus-width = <8>; non-removable;
mmc-hs2-1_2v;//This is the property I added status = "okay"; };

kernel emmc dts

&usdhc2 {
	pinctrl-names = "default", "state_100mhz", "state_200mhz";
	pinctrl-0 = <&pinctrl_usdhc2>;
	pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
	pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
	//cd-gpios = <&gpio4 26 GPIO_ACTIVE_LOW>;
//broken-cd; vmmc-supply = <&reg_usdhc2_vmmc>;
no-1-8v;
disable-wp; bus-width = <4>; status = "okay"; }; &usdhc3 { pinctrl-names = "default", "state_100mhz", "state_200mhz"; pinctrl-0 = <&pinctrl_usdhc3>; pinctrl-1 = <&pinctrl_usdhc3_100mhz>; pinctrl-2 = <&pinctrl_usdhc3_200mhz>; bus-width = <8>;
no-sd;
no-sdio; non-removable;
mmc-hs400-1_8v;
mmc-hs400-emhanced-strobe; status = "okay"; };

 

0 Kudos
Reply