Boot over EMMC 5.1 in I.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot over EMMC 5.1 in I.MX8M

901 Views
dhaval_shah
Contributor II

Hi,

We are working on the I.MX8M chipset based board. We can see from the datasheet that system having I.MX8M can boot over EMMC 5.0 but we don't see anything for 5.1 version.

Is it possible to boot the system over EMMC 5.1.

If possible then can you please point to the file which needs to update to boot over EMMC 5.1

Thanks & Regards,

Dhaval

0 Kudos
4 Replies

745 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhaval

yes it is possible to boot the system over EMMC 5.1, no additional settings/changes 

are needed, ROM falls to emmc 5.0 mode when booting from emmc 5.1.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

745 Views
dhaval_shah
Contributor II

Hi Igor,

Thanks a lot for your quick response.

As I understand from your reply is that, system will use the EMMC 5.0 mode even though booting with EMMC 5.1

So booting over EMMC will never use 5.1 but 5.0 only.

Is my understanding correct?

Thanks & Regards,

Dhaval

0 Kudos

745 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhaval

yes ROM will work as with EMMC 5.0.

Best regards
igor

0 Kudos

745 Views
dhaval_shah
Contributor II

Thanks Igor.

Appreciate your support.

Regards,

Dhaval

0 Kudos