Boot devices support on i.MX8MQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot devices support on i.MX8MQ

Jump to solution
2,133 Views
harshitshah
Contributor III

Hi Team,

 

We checked the supported boot devices of i.MX8MQ. They are as NAND flash and SD/MMC from the RM. However, maybe we have seen in one of the i.MX8MQ schematics we found that there is a configuration for QSPI-NOR flash.

So, just wanted to double confirm, whether i.MX8MQ supports U-boot booting from QSPI-NOR flash? 

Regards

 

Labels (1)
0 Kudos
Reply
1 Solution
2,119 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello harshitshah,

Yes it is supported, Note, for successful boot from new qspi nor specific for that part fspi header in needed, fspi_header:

https://source.codeaurora.org/external/imx/imx-mkimage/tree/scripts?h=imx_5.4.24_2.1.0

Description can be found in sect.5.8.3.3 FlexSPI configuration parameters

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

Regards

View solution in original post

0 Kudos
Reply
2 Replies
2,120 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello harshitshah,

Yes it is supported, Note, for successful boot from new qspi nor specific for that part fspi header in needed, fspi_header:

https://source.codeaurora.org/external/imx/imx-mkimage/tree/scripts?h=imx_5.4.24_2.1.0

Description can be found in sect.5.8.3.3 FlexSPI configuration parameters

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

Regards

0 Kudos
Reply
2,099 Views
harshitshah
Contributor III

Hi @Bio_TICFSL ,

  Thanks for your reply. Looking at the below two images it looks like the secure image flashing only  (and not flashing non-secured one) is supported in i.MX8MQ. Can you please share more information on the same?

 

Regards.

flowchart_for_serial_authentication.PNG

serial_hab.PNG

0 Kudos
Reply