Boot animation timing issue i.MX6 Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot animation timing issue i.MX6 Android

4,285件の閲覧回数
kirangv
Contributor III

I have connected HDMI and LVDS display to i.MX6Q SABRE AI board.

While booting the "android boot animation" is shown at different time on LVDS and HDMI.

First the boot animation is shown on LVDS(primary display) and then after few seconds it starts on HDMI.

I want to start "android boot animation" at the same time on both displays.

Please help on this.

ラベル(4)
11 返答(返信)

3,936件の閲覧回数
houyong
Contributor III

JayTu‌ I got this problem too.It may not be caused by hdmi negotiation delay.I try to execute stop && start in shell to restart android services.The issue also is reproduced. 

0 件の賞賛
返信

3,936件の閲覧回数
JayTu
NXP Employee
NXP Employee

You can try initial HDMI firstly and then LVDS since HDMI needs more time for negotiation, I thought.

0 件の賞賛
返信

3,936件の閲覧回数
houyong
Contributor III

Realy thanks for your reply(nxp email may go before web reply)!We do not have a real lvds lcd,we just adjust hdmi to mxcfb1 to support hdmi hotplug.So blank and unblank operations are invalid to lcd(fake builtin main display).

0 件の賞賛
返信

3,936件の閲覧回数
kirangv
Contributor III

Hi ,

Basically i want both HDMI and LVDS to show contents from boot time unlike only on LVDS as the current scenario.

Is it possible ? 

Thanks,

Kiran

0 件の賞賛
返信

3,936件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The default BSP is the contents on HDMI is scaling from LVDS. You need do some modify the BSP. I will try confirm it for you that if we have such patch. Then give you reply.

Have a nice day

Rita

3,936件の閲覧回数
kirangv
Contributor III

Hi,

Any update would be greatly appreciated.

Thanks,

Kiran

0 件の賞賛
返信

3,936件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Kiran,

The files are large, here I share it with you here:

Kink: http://pan.baidu.com/s/1qYtz2yw

Password: mdn5
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,936件の閲覧回数
kirangv
Contributor III

Hi Rita,

It seems i have received this patch as part of displaying different content on dual display issue.

Please refer - https://community.nxp.com/thread/449536 

patch.PNG

I did applied this patch and still observing HDMI display showing contents late at boot.

Could you please confirm its the same patch or its having fix for both HDMI and LVDS showing contents from boot.

My Issue :

---------------

After booting only LVDS display(on the right) showing contents :

Only_LVDS.PNG

HDMI display (on the left) starts showing contents after 34 seconds from boot :

HDMI_LVDS.PNG

Thanks you for your support on this , greatly appreciated.

Thanks,

Kiran

0 件の賞賛
返信

3,936件の閲覧回数
JayTu
NXP Employee
NXP Employee

TripleDisplay extends android framework and let you specify the screen (LVDS or HDMI) that your image/video will show to. It includes an control UI and service.

Therefore, it starts to work after you launch it.

0 件の賞賛
返信

3,936件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Could you tell me which version BSP are using?

Have a nice day

Rita

0 件の賞賛
返信

3,936件の閲覧回数
kirangv
Contributor III

Hello Rita,

I am using "android_M6.0.1_2.1.0".

Thanks,

Kiran

0 件の賞賛
返信