Boot Problem with Yocto Sumo on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Problem with Yocto Sumo on i.MX6

2,132 Views
claymontgomery
Contributor IV

Hello,

    I'm trying to boot Yocto (2.7) Sumo on a i.MX6 Wandboard Quad (rev d1). It seems to almost work, except at the last step, I get this kernel panic, which I think indicates that the filesystem is not mounted or perhaps is the wrong partition:

            Kernel panic - not syncing: No working init found. 

I built this image according to the instructions in the i.MX_Yocto_Project_User's_Guide, as follows:

    mkdir imx-yocto-bsp
    cd imx-yocto-bsp
    repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
    repo sync

    DISTRO=fsl-imx-fb MACHINE=wandboard source fsl-setup-release.sh -b build-fb
    bitbake fsl-image-machine-test

Note that I did have to change the bootloader_imx name from "u-boot-imx" to "u-boot-fslc" to work on the Wandboard.

I have pasted the entire boot sequence below.

I would appreciate any guidance to resolve this issue.  I will also assist the FSL Community BSP for Wandboard support.

Thanks, Clay


U-Boot SPL 2018.07+fslc+g1e13b91 (Sep 24 2019 - 20:14:11 +0000)
Trying to boot from MMC1


U-Boot 2018.07+fslc+g1e13b91 (Sep 24 2019 - 20:14:11 +0000)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz
Reset cause: POR
I2C:   ready
DRAM:  2 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
auto-detected panel HDMI
Display: HDMI (1024x768)
In:    serial
Out:   serial
Err:   serial
Board: Wandboard rev D1
Net:   FEC [PRIME]
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Found /extlinux/extlinux.conf
Retrieving file: /extlinux/extlinux.conf
195 bytes read in 15 ms (12.7 KiB/s)
1:      NXP i.MX Release Distro
Retrieving file: /extlinux/../zImage
7267608 bytes read in 363 ms (19.1 MiB/s)
append: root=PARTUUID=b6ea8c23-01 rootwait rw console=ttymxc0,115200
Retrieving file: /extlinux/../imx6q-wandboard-revd1.dtb
41637 bytes read in 25 ms (1.6 MiB/s)
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800d2a4

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Tue Sep 24 20:13:14 UTC 2019
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Wandboard i.MX6 Quad Board revD1
Memory policy: Data cache writealloc
Reserved memory: created CMA memory pool at 0x6c000000, size 320 MiB
OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
percpu: Embedded 16 pages/cpu @daef6000 s35532 r8192 d21812 u65536
Built 1 zonelists, mobility grouping on.  Total pages: 520704
Kernel command line: root=PARTUUID=b6ea8c23-01 rootwait rw console=ttymxc0,115200
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 1735132K/2097152K available (9216K kernel code, 498K rwdata, 3204K rodata, 1024K init, 442K bss, 34340K reserved, 327680K cma-reserved, 262144K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
    lowmem  : 0x80000000 - 0xf0000000   (1792 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x80a00000   (10208 kB)
      .init : 0x80e00000 - 0x80f00000   (1024 kB)
      .data : 0x80f00000 - 0x80f7c900   ( 499 kB)
       .bss : 0x80f7e000 - 0x80fec920   ( 443 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
        Tasks RCU enabled.
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU2: Spectre v2: using BPIALL workaround
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
CPU3: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
random: get_random_u32 called from bucket_table_alloc+0x114/0x23c with crng_init=0
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
vdd1p1: supplied by regulator-dummy
vdd3p0: supplied by regulator-dummy
vdd2p5: supplied by regulator-dummy
vddarm: supplied by regulator-dummy
vddpu: supplied by regulator-dummy
vddsoc: supplied by regulator-dummy
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx rpmsg driver is registered.
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usb_phy_generic 2000000.aips-bus:usbphy_nop1: 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
usb_phy_generic 2000000.aips-bus:usbphy_nop2: 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 4, 65536 bytes)
TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
workingset: timestamp_bits=30 max_order=19 bucket_order=0
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
imx-sdma 20ec000.sdma: no iram assigned, using external mem
mxs-dma 110000.dma-apbh: initialized
imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
imx-sdma 20ec000.sdma: Falling back to user helper
pfuze100-regulator 2-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 2-0008: FAB: 0, FIN: 0
pfuze100-regulator 2-0008: pfuze100 found.
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 67, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi host0: ahci-imx
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 74
libphy: Fixed MDIO Bus: probed
CAN device driver interface
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 2184800.usbmisc: 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
ata1: SATA link down (SStatus 0 SControl 300)
ahci-imx 2200000.sata: no device found, disabling link.
ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
random: fast init done
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
caam 2100000.caam: ERA source: CAAMVID.
caam 2100000.caam: AXI pipeline throttling enabled.
caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0, dpaa2 = no
caam_jr 2101000.jr0: Entropy delay = 3200
mmc2: host does not support reading read-only switch, assuming write-enable
mmc1: new high speed SDIO card at address 0001
mmc2: new high speed SDHC card at address aaaa
mmcblk2: mmc2:aaaa SL16G 14.8 GiB
caam_jr 2101000.jr0: Instantiated RNG4 SH0.
 mmcblk2: p1 p2
caam_jr 2101000.jr0: Instantiated RNG4 SH1.
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 43 e1 02 5f 65 b2 90 2c
platform caam_sm: [0008] 49 6b 4a d3 d2 a0 11 8f
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] cf 95 38 18 02 e4 bb 18
platform caam_sm: [0008] c4 68 0d 2c 1b 2b ba 30
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 5c d2 16 a1 59 4c 7e 6e
platform caam_sm: [0008] 21 b9 76 88 48 2d d3 de
platform caam_sm: [0016] 14 cd f9 1a b2 f9 b2 c0
platform caam_sm: [0024] 78 53 34 be fd 00 44 23
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 16 26 2d 48 4f b0 f2 06
platform caam_sm: [0008] 4d 3b d0 97 a9 09 15 1a
platform caam_sm: [0016] 78 e8 a5 0a aa f2 61 6b
platform caam_sm: [0024] 6f 5e 00 00 51 77 26 14
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] a8 63 61 eb 84 cb c6 c4
platform caam_sm: [0008] 6f 6b 8f be 52 f2 2d e2
platform caam_sm: [0016] f4 01 4f 4b cc 42 ab 38
platform caam_sm: [0024] f3 ca 42 a5 db 12 48 66
platform caam_sm: [0032] 21 49 e8 f8 bf f7 0b 12
platform caam_sm: [0040] b6 d9 72 38 87 13 3f 8f
platform caam_sm: [0048] e8 91 72 59 be 10 fd 0a
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 84 78 1d be a7 b4 ea ad
platform caam_sm: [0008] 6b 12 e9 29 fc 74 9f fc
platform caam_sm: [0016] 3c 34 41 58 f5 36 5f d7
platform caam_sm: [0024] 07 a6 d5 33 4e eb 82 14
platform caam_sm: [0032] 1c 5d 87 fe 1f 91 9f a6
platform caam_sm: [0040] 8a 72 7c c7 62 1b 78 82
platform caam_sm: [0048] c4 ee ad b3 66 ea ef 7a
platform caam_sm: [0056] b0 bf 8a 93 da 87 55 e6
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 6c 93 4b cd 38 db f9 00
platform caam_sm: [0008] 22 cd 23 65 dd fb 0b c7
platform caam_sm: [0016] b4 8d ad 15 de 02 74 a5
platform caam_sm: [0024] b6 3c 34 f1 fb 3d d6 82
platform caam_sm: [0032] c8 e0 98 53 49 cb 8c dd
platform caam_sm: [0040] 1e 0a 16 cb 30 98 25 13
platform caam_sm: [0048] a8 21 4a ae 3d 3f 29 38
platform caam_sm: [0056] 29 d9 3c 03 26 7f 11 21
platform caam_sm: [0064] 5f 03 e2 96 a4 d7 f5 f5
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 7e 39 42 42 dd 52 42 fb
platform caam_sm: [0008] 12 5f ff 0f eb 38 96 3f
platform caam_sm: [0016] 23 54 81 81 42 51 16 2a
platform caam_sm: [0024] d1 64 f7 7d fb ac ac 11
platform caam_sm: [0032] 4f 35 8f d6 f1 ee 83 ba
platform caam_sm: [0040] 32 2b 07 61 8a 65 58 a8
platform caam_sm: [0048] 85 e7 34 ce c0 27 5b 1d
platform caam_sm: [0056] 64 0c d1 1d 77 88 21 0a
platform caam_sm: [0064] 63 ef 92 4c c6 39 5a 15
platform caam_sm: [0072] 3a 05 a5 cb 11 6f 5e 6d
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] fe 28 b9 ee 2f 71 7e ba
platform caam_sm: [0008] 62 00 81 47 2b b8 92 20
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] cf 95 38 18 02 e4 bb 18
platform caam_sm: [0008] c4 68 0d 2c 1b 2b ba 30
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 5c d2 16 a1 59 4c 7e 6e
platform caam_sm: [0008] 21 b9 76 88 48 2d d3 de
platform caam_sm: [0016] 9d 0a 1e 3a 90 e8 7d ad
platform caam_sm: [0024] d8 82 d8 82 af 05 49 66
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 16 26 2d 48 4f b0 f2 06
platform caam_sm: [0008] 4d 3b d0 97 a9 09 15 1a
platform caam_sm: [0016] 78 e8 a5 0a aa f2 61 6b
platform caam_sm: [0024] 6f 5e 00 00 51 77 26 14
caam-snvs 20cc000.caam-snvs: can't get snvs clock
caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000 1-000a: Error reading chip id -6
fsl-ssi-dai 2028000.ssi: No cache defaults, reading back from HW
imx-sgtl5000 sound: ASoC: CODEC DAI sgtl5000 not registered
imx-sgtl5000 sound: snd_soc_register_card failed (-517)
imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok
NET: Registered protocol family 26
NET: Registered protocol family 10
Segment Routing with IPv6
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
Key type dns_resolver registered
(NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
imx_thermal 2000000.aips-bus:tempmon: Extended Commercial CPU temperature grade - max:105C critical:100C passive:95C
imx-sgtl5000 sound: ASoC: CODEC DAI sgtl5000 not registered
imx-sgtl5000 sound: snd_soc_register_card failed (-517)
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:04:12 UTC (252)
ALSA device list:
  #0: imx-spdif
FAT-fs (mmcblk2p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
VFS: Mounted root (vfat filesystem) on device 179:1.
devtmpfs: error mounting -2
Freeing unused kernel memory: 1024K
Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.
CPU3: stopping
CPU: 3 PID: 0 Comm: swapper/3 Not tainted 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<8010ef44>] (unwind_backtrace) from [<8010b49c>] (show_stack+0x10/0x14)
[<8010b49c>] (show_stack) from [<809a2da4>] (dump_stack+0x78/0x8c)
[<809a2da4>] (dump_stack) from [<8010dd98>] (handle_IPI+0x198/0x1ac)
[<8010dd98>] (handle_IPI) from [<80101510>] (gic_handle_irq+0x8c/0x90)
[<80101510>] (gic_handle_irq) from [<8010bfcc>] (__irq_svc+0x6c/0xa8)
Exception stack(0xd8097f58 to 0xd8097fa0)
7f40:                                                       00000000 7fffffff
7f60: 00000001 daf31200 b3ea544c 00000000 daf2d4e8 00000001 b39b1c59 00000000
7f80: 00000000 00000000 00000000 d8097fa8 809bc724 806e4100 20000013 ffffffff
[<8010bfcc>] (__irq_svc) from [<806e4100>] (cpuidle_enter_state+0x13c/0x2cc)
[<806e4100>] (cpuidle_enter_state) from [<80162e24>] (do_idle+0x1b8/0x208)
[<80162e24>] (do_idle) from [<8016312c>] (cpu_startup_entry+0x18/0x1c)
[<8016312c>] (cpu_startup_entry) from [<1010180c>] (0x1010180c)
CPU0: stopping
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<8010ef44>] (unwind_backtrace) from [<8010b49c>] (show_stack+0x10/0x14)
[<8010b49c>] (show_stack) from [<809a2da4>] (dump_stack+0x78/0x8c)
[<809a2da4>] (dump_stack) from [<8010dd98>] (handle_IPI+0x198/0x1ac)
[<8010dd98>] (handle_IPI) from [<80101510>] (gic_handle_irq+0x8c/0x90)
[<80101510>] (gic_handle_irq) from [<8010bfcc>] (__irq_svc+0x6c/0xa8)
Exception stack(0x80f01f20 to 0x80f01f68)
1f20: 00000000 daf01200 00000001 daf01200 b3ea51b1 00000000 daefd4e8 00000001
1f40: b39ba276 00000000 00000000 00000000 00000000 80f01f70 809bc724 806e4100
1f60: 20000013 ffffffff
[<8010bfcc>] (__irq_svc) from [<806e4100>] (cpuidle_enter_state+0x13c/0x2cc)
[<806e4100>] (cpuidle_enter_state) from [<80162e24>] (do_idle+0x1b8/0x208)
[<80162e24>] (do_idle) from [<8016312c>] (cpu_startup_entry+0x18/0x1c)
[<8016312c>] (cpu_startup_entry) from [<80e00c5c>] (start_kernel+0x388/0x394)
CPU2: stopping
CPU: 2 PID: 0 Comm: swapper/2 Not tainted 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<8010ef44>] (unwind_backtrace) from [<8010b49c>] (show_stack+0x10/0x14)
[<8010b49c>] (show_stack) from [<809a2da4>] (dump_stack+0x78/0x8c)
[<809a2da4>] (dump_stack) from [<8010dd98>] (handle_IPI+0x198/0x1ac)
[<8010dd98>] (handle_IPI) from [<80101510>] (gic_handle_irq+0x8c/0x90)
[<80101510>] (gic_handle_irq) from [<8010bfcc>] (__irq_svc+0x6c/0xa8)
Exception stack(0xd8095f58 to 0xd8095fa0)
5f40:                                                       00000000 7fffffff
5f60: 00000001 daf21200 b3ea544c 00000000 daf1d4e8 00000001 b39b2429 00000000
5f80: 00000000 00000000 00000000 d8095fa8 809bc724 806e4100 20000013 ffffffff
[<8010bfcc>] (__irq_svc) from [<806e4100>] (cpuidle_enter_state+0x13c/0x2cc)
[<806e4100>] (cpuidle_enter_state) from [<80162e24>] (do_idle+0x1b8/0x208)
[<80162e24>] (do_idle) from [<8016312c>] (cpu_startup_entry+0x18/0x1c)
[<8016312c>] (cpu_startup_entry) from [<1010180c>] (0x1010180c)
---[ end Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.

0 Kudos
Reply
1 Reply

1,748 Views
igorpadykov
NXP Employee
NXP Employee

Hi Clay

one can try nxp linux from source.codeaurora.org/external/imx/linux-imx repository

linux-imx - i.MX Linux kernel 

Linux documentation

i.MX Software | NXP 

Wandboard is not supported by nxp, issue may be posted on wandboard forum

Wandboard Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply