Boot Order when using HAB with a DCD present

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot Order when using HAB with a DCD present

跳至解决方案
1,420 次查看
传策薛
Contributor V

Can send me the document, I also want to use the hab?

0 项奖励
回复
1 解答
1,373 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent  Your some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,374 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent  Your some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
718 次查看
narkoskatona
Contributor II

Could you send also to me, please?

0 项奖励
回复
1,373 次查看
传策薛
Contributor V

Thanks a lot

0 项奖励
回复