Boot Hang issue in iMx8DX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Hang issue in iMx8DX6

2,813 Views
sheraz_ali
Contributor II

Hi Sir,

iMx8DX6 board stops at boot level and after we switch off and on the board it starts working

I have attached the working and non working  logs for your reference

When the boot hangs it stops at the following line

[    1.573346] mmc1: new ultra high speed SDR104 SDIO card at address 0001                          
[    1.608663] cdc_acm 1-1:1.2: ttyACM0: USB ACM device 

[ 1.569061] usb_otg1_vbus: disabling 

The above line is present when the board is booting but not when it hangs ?

Any suggestions why the board is hanging

0 Kudos
Reply
7 Replies

2,492 Views
sheraz_ali
Contributor II

I got DD3 tool from NXP, after editing DDR programming Aid i got the same configuration which i was using earlier. what else would cause the boot hang

0 Kudos
Reply

2,492 Views
igorpadykov
NXP Employee
NXP Employee

only one reliable way to prevent boot hang is reset all board power

(shortly remove all voltages through pmic).

Best regards
igor

0 Kudos
Reply

2,492 Views
sheraz_ali
Contributor II

What do you mean when you say remove all voltages through pmic ?

Secondly How to achieve that via software

0 Kudos
Reply

2,492 Views
igorpadykov
NXP Employee
NXP Employee

>What do you mean when you say remove all voltages through pmic ?

use solution from i.MX8QXP MEK schematic

pastedImage_1.jpg

>Secondly How to achieve that via software

this is not possible.

0 Kudos
Reply

2,491 Views
sheraz_ali
Contributor II

can anyone share the DDR aid tool for DDR3L (iMx8DX6)

0 Kudos
Reply

2,491 Views
igorpadykov
NXP Employee
NXP Employee

Hi sheraz

reason may be ddr memory errors, so one can try to use latest

 i.MX8QXP LPDDR4 Register Programming Aid (MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v13.xlsx)

and rerun ddr test (latest v.13.1) , then rebuild image.

Also one can disconnect SDR104 SDIO card and check if it causes the hang.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,492 Views
sheraz_ali
Contributor II

Hi igorpadykov,

                        I am flashing the flash_a.bin flash_b.bin by running the following commands in Linux side

First copying the flash_a.bin and flash_b.bin to /tmp folder then executing the below commands

dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=4 conv=fsync count=16
sync

echo 0 > /sys/block/mmcblk0boot0/force_ro
dd if=/tmp/flash_a.bin of=/dev/mmcblk0boot0 bs=1k seek=32 conv=fsync
dd if=/tmp/flash_b.bin of=/dev/mmcblk0boot0 bs=1k seek=4096 conv=fsync
echo 1 > /sys/block/mmcblk0boot0/force_ro
sync

Is this method correct or am i missing any steps

Thanks and Regards

Sheraz Ali Shah

0 Kudos
Reply