Hi,
Boost output on the MMPF0100 can be selected between 5.0V/5.05V/5.10V/5.15V using the Register SWBSTCTL - ADDR 0x66, bits SWBST1VOLT.
Max load current is 500 or 600mA (depending on the input voltage), make sure, your load is not demanding more current than the boost can handle.
Note that the parasitic leakage path for a boost regulator causes the SWBSTOUT and SWBSTFB voltage to be a Schottky drop below the input voltage whenever SWBST is disabled.
Make sure SWBT1MODE and SWBSTBYMODE bits are ‘10’ (Auto (default)).
What is the input voltage for the SWBSTIN pin?
SWBSTIN range should be between 2.8V and 4.5V
Regards,
Jose
NXP Semiconductors