BogoMIPS : 3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BogoMIPS : 3.0

953件の閲覧回数
jialu
Contributor II

1.jpg

Why BogoMIPS is 3.00? What does 3.00 means?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

836件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi XU

please look on

BogoMips - Wikipedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

836件の閲覧回数
jialu
Contributor II

Just 3.00?

In my PC, it's value is 5184.00.

Is there some thing wrong here?

3Q

0 件の賞賛
返信

836件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

you can try kernel 3.0.35 which had correct value.

change happens since:  commit 1119c84aa3053bd415ba731ada1ecef24c8f82a2
Author: Sebastian Andrzej Siewior <bigeasy@linutronix.de>
Date: Wed Jan 22 12:35:44 2014 +0100

ARM: imx: enable delaytimer on the imx timer

The imx can support timer-based delays, so implement this.
Skips past jiffy calibration.

0 件の賞賛
返信