We have i.MX 6DualLite SABRE Smart Device.
BSP: fsl-bsp-relase rocko
Board reset when running GPU test.
root@imx6dlsabresd:/unit_tests/GPU# ./gpu.sh
---- Running < gpu.sh > test ----
/unit_tests/GPU /unit_tests/GPU
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1bf9f (Mar 20 2020 - 11:27:09
+0530)
CPU: Freescale i.MX6DL rev1.1 996 MHz (running at 792 MHz)
CPU: Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: Freescale i.MX6 DualLite SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Solved! Go to Solution.
Hello Nilesh
I tested on my side with MX6Q and sabre board and no reset was found even with qt webengine, I´m using 4.14.78 BSP.
Regards
Thanks for your valuable input.
This is power supply issue and after changing power supply then no more device reset.
Thanks for reply
I have tested using warrior-4.19.35-1.1.0
README\imx - meta-fsl-bsp-release - i.MX Yocto Project Release Layer
But same result.
Board reset when running GPU test.
Same result occurs when running qt webengine.
Hello Nilesh
I tested on my side with MX6Q and sabre board and no reset was found even with qt webengine, I´m using 4.14.78 BSP.
Regards
Hello Niless,
The error is present in that particular BSP, please change you BSP to the new one L4.19.35 or L4.14.78.
Regards