Bluetooth: unable to receive files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth: unable to receive files

860 Views
DC95
Contributor I

I use the imx8mmini board (Linux version 4.14.98)

When i test bluetooth, use the following command:

# bluetoothctl

[bluetooth]# power on

[bluetooth]# pairable on

[bluetooth]# discoverable on

[bluetooth]# scan on

[bluetooth]# pair 22:22:C6:AB:48:DB

[bluetooth]# trust 22:22:C6:AB:48:DB

[bluetooth]# quit

# export $(dbus-launch)

# /usr/libexec/bluetooth/obexd -r /home/root -a -d & obexctl

[obex]# connect 22:22:C6:AB:48:DB

[22:22:C6:AB:48:DB]# send /home/root/123.png

Now, picture can be transferred to the tablet via bluetooth.

But when I transfer files to the board through the tablet, it can't.

Why is it identified as a Bluetooth headset device???

0601.jpg

 

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies