Bluetooth on Wandboard using freescale "fsl-image-machine-test" with yocto 1.7.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth on Wandboard using freescale "fsl-image-machine-test" with yocto 1.7.1

694 Views
andrewjimenez
Contributor I

Hello,

This is my first time posting so I hope I am doing this right :smileyhappy:

I have been trying to get bluetooth working on a wandboard-dual (Rev A0) on Yocto 1.7.1 for the last few weeks and have run into issue after issue. At this point I am having a hard time even making the hci device show up, even with brcm-patchram-plus and loading the correct drivers. The image I am testing this on is the "fsl-image-machine-test” image, which I have made no modifications to. The few times I have gotten the bluetooth device to show up, I realized that my image did not have any of the bluez tools (bluez-simple-agent) installed, even though I believe they should have been. Has anyone faced these issues or have any tips for how I should continue?

Thanks!

0 Kudos
Reply
0 Replies