Bluetooth card reset issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth card reset issue.

1,523 Views
Rajput1z
Contributor II

Hello,

I am using custom hardware is based on i.MX535 Sabre platform

1. Bluetooth is connected to UART3 and communicate with chip based on BCSP protocol .

2. Scanning is ok.

3. File transfer , and BT audio over SCO also ok.

BUT, some times while file transferring or in BT voice call time i am getting  error

bcsp_pkt_cull: Peer acked invalid packet

bcsp_handle_le_pkt: Found a LE sync pkt, card has reset

please advice how to resolve this issue .

Regards,

suman.

Labels (1)
0 Kudos
Reply
1 Reply

1,234 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rajput

seems this is well know bug in BT stack, please refer to links below

How to run up CSR chip without eeprom with BLUEZ ? -- Bluez Devel

bluez - bluetooth stack for Linux - users

Probably more updated BT driver on newer kernel will help

i.MX53 Quick Start - Linux on ARM - eewiki

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply