Bluetooth NINA-B410 HCi interface not able to initialize with IMX8XQP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluetooth NINA-B410 HCi interface not able to initialize with IMX8XQP

489 次查看
Akshaya
Contributor II
-When iam trying to initialize the HCI interface it is showing timeout error 
 
-sudo hciattach /dev/ttyLP1 any 115200 noflow
output
-Setting TTY to N_HCI line discipline
-Device setup complete
-[ 656.751608] Bluetooth: hci0: command 0x1003 tx timeout
 
-When iam trying to know the status of hci interface it is giving me 
-hciconfig
output
-hci0: Type: Primary Bus: UART
BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0
DOWN
 
-When iam trying to up the hci config also the above time out error is occuring 
-I tried to enable all the required drivers if required in kernel then also the timeout issue still persisit .
 
-Trying to findout what is causing the timeout issue and how to solve it .
 
 
 
 
0 项奖励
回复
2 回复数

470 次查看
Chavira
NXP TechSupport
NXP TechSupport

HI @Akshaya!

Thank you for contacting NXP Support!

 

Unfortunately we don't know what the problem could be since is a Nordic Semiconductor chip.

I recommend contacting Nordic Semiconductor support or U-BLOX support to get the driver.

 

Also if the problem persists you can use one of our wifi solutions and are already integrated in our BSP.

 

Best Regards!

Alejandro

0 项奖励
回复

436 次查看
Akshaya
Contributor II

Hi @Chavira,

Thank you for your response!

If you come across any information regarding this issue, please let me know.

Best regards,
Akshaya