Bluetooth Audio playback on Jellybean

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth Audio playback on Jellybean

1,295 Views
johnturnur
Contributor III

Hi,

What changes are required to enable Bluetooth playback on Jellybean using imx6q SABRE SDB board?

Find log as below:-

E/BluetoothAdapterState( 2884): Error enabling Bluetooth

D/BluetoothAdapterService( 2884): Broadcasting updateAdapterState() to 1 receivers.

D/BluetoothManagerService( 2579): Message: 60

D/BluetoothManagerService( 2579): MESSAGE_BLUETOOTH_STATE_CHANGE: prevState = 11, newState=10

D/BluetoothManagerService( 2579): Broadcasting onBluetoothStateChange(false) to 8 receivers.

D/BluetoothPbap( 2848): onBluetoothStateChange: up=false

D/BluetoothHeadset( 2745): onBluetoothStateChange: up=false

D/BluetoothHeadset( 2745): onBluetoothStateChange: up=false

D/BluetoothInputDevice( 2848): onBluetoothStateChange: up=false

D/BluetoothHeadset( 2579): onBluetoothStateChange: up=false

D/BluetoothA2dp( 2579): onBluetoothStateChange: up=false

D/BluetoothManagerService( 2579): Bluetooth State Change Intent: 11 -> 10

D/BluetoothAdapterService(1091503048)( 2884): getState(): mAdapterProperties: com.android.bluetooth.btservice.AdapterProperties@410f1cf0

W/ContextImpl( 2848): Calling a method in the system process without a qualified user: android.app.ContextImpl.startService:1352 android.content.ContextWrapper.startService:450 android.content.ContextWrapper.startService:450 com.android.settings.bluetooth.DockEventReceiver.beginStartingService:134 com.android.settings.bluetooth.DockEventReceiver.onReceive:115

D/DockEventReceiver( 2848): finishStartingService: stopping service

D/BluetoothAdapterService(1091503048)( 2884): getState(): mAdapterProperties: com.android.bluetooth.btservice.AdapterProperties@410f1cf0

-John

0 Kudos
4 Replies

736 Views
johnturnur
Contributor III

Hi

How can i get Bluetooth Working in Jellybean?

0 Kudos

736 Views
raymondwang
Senior Contributor I

     After android 4.2. The bluetooth stack changed to new Bluedroid stack which is located in /external/bluetooth/bluedroid.

This is android hardware module implementation for android bluetooth stack. This stack will trying to load a vendor library

named libbt-vendor.so.You need to implement your bluetooth chip library.

   Android source tree has an example to implement the library in /device/common/libbt. Specially this is broadcom based

BT chipset. It's easy to modify it to support your bluetooth chip. The important things about this library are how to access

your HCI port and how to control Bluetooth RF.

  Good luck!

0 Kudos

736 Views
mutyalaraoneela
Contributor III

Hi Raymond Wang,

Plat form IMX6SL

bluedroid on adroid kitkat 4.4.3

  I have  2 issues one while data transfer, the other while enabling via GUI.

   1) After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :

   File not Received

   File : sample.jpg

   Reason : Storage issue

  2) And presently I am inserting my driver via GUI, I am getting an error message while enabling bluetooth via GUI   ie Operation not permitted while loading .ko (driver)Please suggest me what to do?? whether I need to install my driver at boot by adding in init.rc?? if I do it always on boot bt will be in ON State only??  OR Do i need to build my driver along with android source code???

Please suggest me how to proceed further???

Thanks and Regards,

Mutyala Rao.

0 Kudos

736 Views
raymondwang
Senior Contributor I

FYI. All my source tree located at xhteam · GitHub

device-fsl/qpad_6dq at imx_jb · xhteam/device-fsl · GitHub 

is my board definition directory. It's long time since my developing work almost finished.

And I can't remember when I insert .ko file (init.xxx.rc or in single program)

Hope this can help you.

0 Kudos