Blank screen on connecting to LVDS to imx8mm for Android 10 OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Blank screen on connecting to LVDS to imx8mm for Android 10 OS

2,715 次查看
Ruban1
Contributor II

Blank screen on connecting to LVDS to imx8mm for Android 10 OS .Throught the recommended chip suggest by the NXP . SN65DSI83TPAPRQ1 . Only the touch is working and back light is working .But the screen is blank. Should i enable any config . Or do you have any  steps followed for Android 10 OS to support mipi to LVDS.  

0 项奖励
回复
8 回复数

2,705 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ruban

 

unfortunately SN65DSI83 is not supported in NXP BSPs, one can look at example on below

link and port it to Android

https://variwiki.com/index.php?title=DART-MX8M-MINI_Display

 

Best regards
igor

0 项奖励
回复

2,668 次查看
Ruban1
Contributor II

how to enable LVDS. can you tell me in which file should i enable first and will the mipi port be compatible with both LVDS and HDMI or should i disable other one to enable.

0 项奖励
回复

2,661 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

2,590 次查看
Ruban1
Contributor II

Hi Igor,

         From the Link which you have sent .In the topic 

"Definition of the SN65DSI83"

the entire function from i2c3

Where should i place that function. Because his not mentioned anything about that. Should i place in Kernel dts or U boot dts or in any patch. Because i gone through their dts file both kernel and uboot. It was not added. I am not able to find out which path they have added.

Kindly Support

Thanks and regards 

Ruban

0 项奖励
回复

2,674 次查看
Ruban1
Contributor II

for configuring according to link you have provided. Should i edit or should i add the snippet code.

And in which file should i add or edit in imx8mm-evk.dts file or imx8mm-evk.dtsi file . And for all the config should i do with standard or with the LVDS distibuter according to the display  

0 项奖励
回复

2,696 次查看
Ruban1
Contributor II

The link you have suggest is only for yocto and debian.

In the link if you scroll down to last . you will find Categories which it will support

It doesn't support to Android OS

0 项奖励
回复

2,690 次查看
igorpadykov
NXP Employee
NXP Employee

Android is based on linux, so that link is relevant to your case.

 

Best regards
igor

0 项奖励
回复

2,687 次查看
Ruban1
Contributor II

for configuring according to link you have provided. Should i edit or should i add the snippet code.

And in which file should i add or edit in imx8mm-evk.dts file or imx8mm-evk.dtsi file . And for all the config should i do with standard or with the LVDS distibuter according to the display  

0 项奖励
回复