Blank display in imx8mm using LVDS bridge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blank display in imx8mm using LVDS bridge

421件の閲覧回数
Ruban1
Contributor II

Hi sir/ madam,

    I am currently working on Imx8mm LVDS display using sn65dsi83 mipi to lvds converter.

The problem i am facing is . I am able to attach the driver and able to probe the driver .

The current doubt is is it enough for me only to probe with LVDS bridge driver or should i even add the panel files also.

If i have to add panel files. I have already configure panel-simple.c file according to my requirements but the problem is i am not able to enter the panel folder .. I checked using added printk msg but not even one is displayed .

Kindly help me to solve the solution

 

Thanks and regards

Ruban

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

416件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛