Bitbaking Linux-Wandboard ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bitbaking Linux-Wandboard ?

990 次查看
mustafabakircio
Contributor IV

Hello;

I have a made the changes on the mxc_mipi_csi2.c file to adjust right clock configuration in the  linux-wandboard  directory.

I think I using bitbake command ,which is

bitbake -c compile -f virtual/kernel then

then

bitbake -c deploy virtual/kernel

after that  I am using ;

bitbake core-image-base    

to create my image but I think I am doing wrong , so I couldnt get the csi_mclk .

What am I doing wrong with this command ? Can you help me .

Thanks

Best Regards

Mustafa

标记 (4)
0 项奖励
回复
1 回复

823 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mustafa

please look at

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------