Bitbake not installing files from recipe to rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bitbake not installing files from recipe to rootfs

跳至解决方案
10,998 次查看
neuro
Contributor III

Hello!

I'm currently using yocto to build the system imx6sxsabresd (IMX6 Solo X). I have successfully built the image however I want to add some a script to init.d to turn on a led. I'm appending to the linux-imx recipes.

This is my linux-imx.bbappend file:

FILESEXTRAPATHS_prepend := "${THISDIR}/linux-imx:"

SRC_URI += "file://0001-added-pad-for-heartbeat-led.patch \
        file://heartbeat.sh \
        file://heartbeat "

PACKAGECONFIG_append = " heartbeat"

inherit update-rc.d
INITSCRIPT_PACKAGES = "${PN}"
INITSCRIPT_PARAMS = "start"
INITSCRIPT_NAME = "heartbeat.sh"

do_install_append() {
  install -d ${D}${sysconfdir}/init.d
  install -m 0755 ${WORKDIR}/heartbeat.sh ${D}${sysconfdir}/init.d/heartbeat.sh

  install -d ${D}/home/root
  install -m 0755 ${WORKDIR}/heartbeat ${D}/home/root/heartbeat
}

FILES_${PN} += "${sysconfdir}/init.d/heartbeat.sh /home/root/heartbeat"
PACKAGES = "${PN}"

I'm able to create the sdcard image succesfully with the patch I've included in this bbappend file, however, the files heartbeat.sh and heartbeat are not copying to the final rootfs added to the output sdcard file. This is very odd because I'm able to see these files in their paths copied to ../tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/4.14.98-r0/image/

标签 (4)
1 解答
10,136 次查看
karangajjar
Senior Contributor II

Hi Jon Clay,

Please add following line to your <build_dir>conf/local.conf file:

IMAGE_INSTALL_append = " <recipe_name>"   

Let us know in case of any concern.

Regards,

Karan Gajjar

在原帖中查看解决方案

0 项奖励
回复
4 回复数
10,137 次查看
karangajjar
Senior Contributor II

Hi Jon Clay,

Please add following line to your <build_dir>conf/local.conf file:

IMAGE_INSTALL_append = " <recipe_name>"   

Let us know in case of any concern.

Regards,

Karan Gajjar

0 项奖励
回复
10,136 次查看
neuro
Contributor III

Hi, I tried this and it works.

Sorry for the delay in response.

Thank you!!

10,136 次查看
karangajjar
Senior Contributor II

Hi Jon Clay,

We are glad you have fixed the issue. Let us know in case of any more concerns.

Regards,

Karan Gajjar

0 项奖励
回复
10,136 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jon Clay,


Is the problem still present? The procedure you followed looks correct. However, have you checked the priority of the layer in which your append is located? It could be that it's been overwritten by some other instruction or append if the priority is not high enough.

Regards,

0 项奖励
回复