Dear Community,
I'm bitbaking full image for imx8mpevk with BSP-5.4.70-2.3.2 and struggling with following error :
ERROR: onnxruntime-1.5.3-r0 do_unpack: gitsm: submodule unpack failed: UnpackError Unpack failure for URL: 'gitsm://github.com/onnx/onnx;protocol=https;name=cmake/external/onnx;subpath=cmake/external/onnx;bareclone=1;nobranch=1'. No up to date source found: clone directory not available or not up to date: /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/../../NXP/Boards/Common/Yocto/yocto_dl/v5.4//git2/github.com.onnx.onnx; shallow clone not enabled
ERROR: onnxruntime-1.5.3-r0 do_unpack: Unpack failure for URL: 'gitsm://github.com/onnx/onnx;protocol=https;name=cmake/external/onnx;subpath=cmake/external/onnx;bareclone=1;nobranch=1'. No up to date source found: clone directory not available or not up to date: /workdir/Dynimlabs/spark-yocto-bsp-5_4_70-2_3_2/../../NXP/Boards/Common/Yocto/yocto_dl/v5.4//git2/github.com.onnx.onnx; shallow clone not enabled
ERROR: Logfile of failure stored in: /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/build-xwayland/tmp/work/aarch64-poky-linux/onnxruntime/1.5.3-r0/temp/log.do_unpack.16020
ERROR: Task (/workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.5.3.bb:do_unpack) failed with exit code '1'
WARNING: armnn-onnx-1.3.0-r0 do_fetch: Failed to fetch URL git://github.com/onnx/onnx.git, attempting MIRRORS if available
ERROR: armnn-onnx-1.3.0-r0 do_fetch: Fetcher failure: Unable to find revision bae6333e149a59a3faa9c4d9c44974373dcf5256 in branch master even from upstream
ERROR: armnn-onnx-1.3.0-r0 do_fetch: Fetcher failure for URL: 'git://github.com/onnx/onnx.git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/build-xwayland/tmp/work/aarch64-poky-linux/armnn-onnx/1.3.0-r0/temp/log.do_fetch.16006
ERROR: Task (/workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx_1.3.0.bb:do_fetch) failed with exit code '1'
Meanwhile I cloned above repositories and checkouted the commits found in related recipes without problem.
Have you ever seen this issue?
My host is Ubuntu-1804 (docker container).
Thanks and best regards,
Khang.
解決済! 解決策の投稿を見る。
Hi Khang,
The Problem is because of the branch name. Branch name should the main not master (Since Github default branch name changed to main), if not mentioned it will look for master.
So change the SRC_URI in /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx_1.3.0.bb as below.
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
Regards,
Sanjaikumar
yes i do L5.10.35 ok
i @josephzhou1 ,
Thanks for your answer but I'm looking for the solution of BSP-5.4.70-2.3.2 that we are using. Anyway, I could compare and hopefully I could port the changes from your version back to that BSP version.
Regards,
K.
Hi Khang,
You need to specify the branch main in onnxruntime_1.5.3.bb . From the above error logs,it looks like trying to download subpath from the same repository above mentioned.
Regards,
Sanjaikumar
Hi @sanjaikumar ,
As I mentioned earlier, the URI of onnxruntime is : https://source.codeaurora.org/external/imx/onnxruntime-imx/
ONNXRUNTIME_SRC ?= "gitsm://source.codeaurora.org/external/imx/onnxruntime-imx.git;protocol=https"
SRCBRANCH = "imx_5.4.70_2.3.2"
There's no branch main of that package's repository. And the branch imx_5.4.70_2.3.2 well exists.
The onnxruntime repository composes of different submodules, including onnx as below :
[submodule "cmake/external/onnx"]
path = cmake/external/onnx
url = https://github.com/onnx/onnx
I would say the issue is from above. I tried to put branch = main in /workdir/L4ES/imx-yocto-bsp-5_4_70-2_3_2/build-xwayland/tmp/work/aarch64-poky-linux/onnxruntime/1.5.3-r0/git/.gitmodules like following :
[submodule "cmake/external/onnx"]
path = cmake/external/onnx
url = https://github.com/onnx/onnx
branch = main
but the .gitmodules is ovveridden each time I continue bitbaking.
Best Regards,
K.
Hi @sanjaikumar ,
I do not found the relevant info in onnxruntime_1.5.3.bb.There's only following SRC_URI :
ONNXRUNTIME_SRC ?= "gitsm://source.codeaurora.org/external/imx/onnxruntime-imx.git;protocol=https"
SRCBRANCH = "imx_5.4.70_2.3.2"
I believe that it comes from below : https://source.codeaurora.org/external/imx/onnxruntime-imx/tree/.gitmodules?h=imx_5.4.70_2.3.2
Do you kow how to patch it ?
Thanks,
K.
Hi Khang,
The Problem is because of the branch name. Branch name should the main not master (Since Github default branch name changed to main), if not mentioned it will look for master.
So change the SRC_URI in /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx_1.3.0.bb as below.
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
Regards,
Sanjaikumar
Hi @sanjaikumar ,
Thanks for your support. Then it works for armnn-onnx but I still faced with following issue of onnxruntime :
ERROR: onnxruntime-1.5.3-r0 do_unpack: gitsm: submodule unpack failed: UnpackError Unpack failure for URL: 'gitsm://github.com/onnx/onnx;protocol=https;name=cmake/external/onnx;subpath=cmake/external/onnx;bareclone=1;nobranch=1'. No up to date source found: clone directory not available or not up to date: /workdir/Dynimlabs/spark-yocto-bsp-5_4_70-2_3_2/../../NXP/Boards/Common/Yocto/yocto_dl/v5.4//git2/github.com.onnx.onnx; shallow clone not enabled
ERROR: onnxruntime-1.5.3-r0 do_unpack: Unpack failure for URL: 'gitsm://github.com/onnx/onnx;protocol=https;name=cmake/external/onnx;subpath=cmake/external/onnx;bareclone=1;nobranch=1'. No up to date source found: clone directory not available or not up to date: /workdir/Dynimlabs/spark-yocto-bsp-5_4_70-2_3_2/../../NXP/Boards/Common/Yocto/yocto_dl/v5.4//git2/github.com.onnx.onnx; shallow clone not enabled
ERROR: Logfile of failure stored in: /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/build-xwayland/tmp/work/aarch64-poky-linux/onnxruntime/1.5.3-r0/temp/log.do_unpack.10853
ERROR: Task (/workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/onnxruntime/onnxruntime_1.5.3.bb:do_unpack) failed with exit code '1'
Do you know how to resolve, please ?
Khang
Indeed this issue is fixed since 5.10.35-2.0.0 where the branch name is specified.
On 5.4.70-2.3.0 (and earlier than 5.10.35-2.0.0) you need to modify SRC_URI in the recipe:
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
Hi @joanxie ,
So change the SRC_URI in /workdir/L4ES/spark-yocto-bsp-5_4_70-2_3_2/sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx_1.3.0.bb as below.
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
For armnn-onnx, I did modify above recipe (just after the issue had happened), then I got issue with onnxruntime. I think I will try bitbaking from scratch after above modification.
Best Regards,
K.
Hi @sanjaikumar and @joanxie ,
I do not know if there's still something missing but unfortunately your suggestion seems not enough to resolve the issue of bitbaking onnxruntime.
Best Regards,
K.
I suggest that you delete these packages and build again, I don't find this issue before, I don't know if you change something
Hi @joanxie ,
I did remove the whole build-xwayland folder as well. I might try from repo syncing but I do not see any difference aside from a clean sources folder.
Best Regards,
K.
give me all of your build steps, let me reproduce this on my side
Hi @joanxie ,
Step #1 : Create bsp folder and move to inside
mkdir imx-yocto-bsp && cd imx-yocto-bsp
Step #2 : Sync the bsp source code
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.2.xml
Step #3 : Setup the build environment
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-xwayland
Step #4 : Add branch=main into armnn-onnx recipe
vi ../sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn-onnx_1.3.0.bb
...
SRC_URI = "git://github.com/onnx/onnx.git;branch=main"
...
Step #5 : Bitbake full image
bitbake imx-image-full
Best Regards,
K.
hello,
step#2 should have 1 more command
repo sync
please try it out , if OK please set as solution, thank you
Hi @josephzhou1 ,
That was my typo. Of course step #2 includes repo sync. Without it, it is impossible to bitbake. So your suggestion is unfortunately NOT a solution, sorry. But thank you anyway for pointing out the missing command.
Regards,
K.
I have built the bsp successfully
only one error for the onnxruntime, after I change the SRC_URI, I don't get other errors
Hi @joanxie ,
Do you confirm that you changed the SRC_URI of armnn-onnx recipe or onnxruntime recipe, please ?
Best Regards,
K
change this:
armnn-onnx_1.3.0.bb
Hi @joanxie ,
Finally I figure out the issue: even-though I re-do everything from scratch as per steps I provided you, armnn-onnx and onnxruntime packages are still unchanged in separate download folder :
DL_DIR ?= "/workdir/NXP/Boards/Common/Yocto/yocto_dl/v5.4/"
Together with the appending of "branch=main" into SRC_URI within armnx-onnx recipe, removing them from the separate download folder to force a new download of both packages solves the issue.
Thanks for your support!
K.