Bitbake for imx-full-image is failing for FRDM imx93 development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bitbake for imx-full-image is failing for FRDM imx93 development board

769件の閲覧回数
Aditya_Vashista
Contributor II

Hello,

I am trying to build imx-full image using bitbake for imx93, i am following steps mentioned on the getting started page-3 of nxp frdm board imx93.

I am getting the following error:


adi@adi:/storage/POC/imx_yocto_bsp/frdm-imx93$ bitbake imx-image-full
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |####################################################################################| Time: 0:00:01
Loaded 5720 entries from dependency cache.
Parsing recipes: 100% |##################################################################################| Time: 0:00:00
Parsing of 3644 .bb files complete (3643 cached, 1 parsed). 5721 targets, 683 skipped, 17 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx93frdm"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:f43f393ef0246b7bee6eed8bcf8271cf2b8cdf40"
meta-oe
meta-multimedia
meta-python = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-freescale = "HEAD:0f8091c63dd8805610c09b08409bc58492a3b16f"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:04f1f31722751671440c1ed0ad471e2ea3abc1f5"
meta-nxp-demo-experience = "HEAD:8fd7154c05b716e9635279047f65785399432d88"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:783becb4b5716d989f50db95b7133d38eae5b47b"
meta-arm
meta-arm-toolchain = "HEAD:1b85bbb4cab9658da3cd926c62038b8559c5c64e"
meta-clang = "HEAD:fe561f41aef0cff9e6f96730ab59f28dca2eb682"
meta-gnome
meta-networking
meta-filesystems = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:6a80f140e387621f62964209a2e07d3bcfb125ce"
meta-imx-bsp
meta-nxp-demo-experience = "lf-6.6.36-2.1.0:ee1376a89478686a850aa0545695340fe360fa5b"

Sstate summary: Wanted 5686 Local 0 Mirrors 0 Missed 5686 Current 1383 (0% match, 19% complete)# | ETA: 0:00:00
Removing 294 stale sstate objects for arch imx93frdm: 100% |#############################################| Time: 0:00:05
Removing 16 stale sstate objects for arch allarch: 100% |################################################| Time: 0:00:00
Removing 9 stale sstate objects for arch x86_64: 100% |##################################################| Time: 0:00:00
Removing 935 stale sstate objects for arch armv8a: 100% |################################################| Time: 0:00:03
NOTE: Executing Tasks
ERROR: voiceui-voiceplayer-1.0-r0 do_patch: ExecutionError('/storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/temp/run.do_patch.457669', 1, None, None)
ERROR: Logfile of failure stored in: /storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/temp/log.do_patch.457669
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/storage/POC/imx_yocto_bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_populate_sysroot', 'virtual:native:/storage/POC/imx_yocto_bsp/sources/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['gettext-minimal-native', 'libtool-native', 'quilt-native', 'texinfo-dummy-native', 'patch-native', 'attr-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_patch
| mv: cannot stat '/storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/0001-Change-Recipe-Target-Sysroot-path.patch': No such file or directory
| WARNING: exit code 1 from a shell command.
ERROR: Task (/storage/POC/imx_yocto_bsp/sources/meta-nxp-demo-experience/recipes-examples/imx-voice-player/voiceui-voiceplayer.bb:do_patch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 5114 tasks of which 4266 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/storage/POC/imx_yocto_bsp/sources/meta-nxp-demo-experience/recipes-examples/imx-voice-player/voiceui-voiceplayer.bb:do_patch
Summary: There was 1 WARNING message.
Summary: There was 1 ERROR message, returning a non-zero exit code.

 

I am using Ubuntu 24.04 (i know it's recommended to use Ubuntu 22.04, but i am instructed to perform all steps on 24.04). The error seems to be related to a missing patch file. I searched the patch file on my system, but can't find it. Also, i checked if the /frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/git git folder was upto date or not, but it is 

 

adi@adi:/storage/POC/imx_yocto_bsp/frdm-imx93$ cd /storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/git
adi@adi:/storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/git$ git status
On branch MM_04.09.00_2405_L6.6.y
Your branch is up to date with 'origin/MM_04.09.00_2405_L6.6.y'.

nothing to commit, working tree clean
adi@adi:/storage/POC/imx_yocto_bsp/frdm-imx93/tmp/work/armv8a-poky-linux/voiceui-voiceplayer/1.0/git$ git pull
Already up to date.

 

Earlier i was getting error in qt_base module (logs for that present in attached file), so i resolved that by removing ptest from /frdm-imx93/conf/local.conf file.

Please support on this. Thanks in advance

 

Regards

Aditya

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

754件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Aditya_Vashista!

Thank you for contacting NXP Support!

 

Do you have the needed packages to compile the Yocto Project?

 

Try updating and installing the the needed packages with the next commands:

$ sudo apt update 

$ sudo apt upgrade -y

$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils
iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file
locales libacl1

 

What are the full steps that are you following to compile for frdm board?

 

To compile without errors we recommend 4GB of ram for each core of your computer.

You can limit the tasks to compile adding the next lines to your local.conf file

BB_NUMBER_THREADS = "4"
PARALLEL_MAKE = "-j 4"

 

Best Regards!

Chavira

 

0 件の賞賛
返信

749件の閲覧回数
Aditya_Vashista
Contributor II

Hello Chavira,

I have already installed the mentioned packages while setting up the system for Yocto.

 

I have tried parallel threads in combination of 4,8 and 12. But I am getting same errors.

0 件の賞賛
返信

720件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Aditya_Vashista!

 

I am not able to try in Ubuntu 24 since my VM is Ubuntu 22 and is compiling without errors, please try installing Ubuntu 22

 

 

0 件の賞賛
返信