Bit settings file for iMX28EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bit settings file for iMX28EVK

4,079件の閲覧回数
x10
Contributor V

Hi, all

 

I try to find the OTP bit seettings file for iMX28EVK to understand the function of those eFuse bits. Thanks in advance.

 

BR

 

 

Cheng Shi

emtronix

0 件の賞賛
返信
7 返答(返信)

3,190件の閲覧回数
admin
Specialist II

OTP Registers

EVKRAW Chip
HW_OCOTP_CUST00x9F0135C00x00000000
HW_OCOTP_CUST10x9F0135C10x00000000
HW_OCOTP_CUST20x000000000x00000000
HW_OCOTP_CUST30x000000000x00000000
HW_OCOTP_CRYPTO00x000000000x00000000
HW_OCOTP_CRYPTO10x000000000x00000000
HW_OCOTP_CRYPTO20x000000000x00000000
HW_OCOTP_CRYPTO30x000000000x00000000
HW_OCOTP_CUSTCAP0x000000000x00000000
HW_OCOTP_LOCK0x000C00000x000C0000
HW_OCOTP_ROM00x000000000x00000000
HW_OCOTP_ROM10x000000000x00000000
HW_OCOTP_ROM20x000000000x00000000
HW_OCOTP_ROM30x000000000x00000000
HW_OCOTP_ROM40x000000000x00000000
HW_OCOTP_ROM50x000000000x00000000
HW_OCOTP_ROM60x000000000x00000000
HW_OCOTP_ROM70x001001000x00100000
HW_OCOTP_SRK00x000000000x00000000
HW_OCOTP_SRK10x000000000x00000000
HW_OCOTP_SRK20x000000000x00000000
HW_OCOTP_SRK30x000000000x00000000
HW_OCOTP_SRK40x000000000x00000000
HW_OCOTP_SRK50x000000000x00000000
HW_OCOTP_SRK60x000000000x00000000
HW_OCOTP_SRK70x000000000x00000000
0 件の賞賛
返信

3,190件の閲覧回数
x10
Contributor V

MfgTool can send data to UUT which will either call fmd's DeviceIoControl to program data into CUST0 or call routines in otp.c to program directly. My imx28 based board is running CE6.0.

Marc coussement said:

How, can we use Mfgtool to program HW_OCOTP_CUST0 OTP register?

 

Marc,
 

0 件の賞賛
返信

3,190件の閲覧回数
MarcCoussement
Contributor I

How, can we use Mfgtool to program HW_OCOTP_CUST0 OTP register?

 

Marc,
 

0 件の賞賛
返信

3,190件の閲覧回数
x10
Contributor V

With the new release 1.6.2.048, the MAC issue should be settled down. Thanks!

0 件の賞賛
返信

3,190件の閲覧回数
StanleyLee
NXP Employee
NXP Employee

BitInit.exe is feasible but not recommended. Mfgtool can do it, too.  You can finish all your work using Mfgtool, this is very important in factory environment.

0 件の賞賛
返信

3,190件の閲覧回数
x10
Contributor V

Thanks for your reply.

I plan to burn the MAC address to HW_OCOTP_CUST0 with tool BitInit.exe one by one at first, and then program the images of eboot.sb and nk.nb0 into my iMX28 based board with MfgTool.

 

BR

 

Cheng Shi

emtronix

0 件の賞賛
返信

3,187件の閲覧回数
ChrisWilliamson
Contributor III

This  is all I could find. Hopefully what you are lookng for is in here somewhere.

 

Chris

0 件の賞賛
返信