Binder transaction failed on Wandboard. RAM fault?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Binder transaction failed on Wandboard. RAM fault?

1,184 次查看
gaun
Contributor II

Hi,


I had booted Android on my Wandboard (an i.mx6 dual) before and I did not face any problems. Today when I booted up my wandboard I get a lot of binder transaction "transaction failed 29189" and "binder_alloc_buf, no vma" errors and my UI keeps crashing. Is it because of some fault in the RAM? If yes, how can I test the RAM on my Wandboard?

Thanks,

Gautam.

标签 (3)
0 项奖励
回复
1 回复

980 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gautam

please refer to ddr tester tool

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复