Binder transaction failed on Wandboard. RAM fault?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Binder transaction failed on Wandboard. RAM fault?

1,291件の閲覧回数
gaun
Contributor II

Hi,


I had booted Android on my Wandboard (an i.mx6 dual) before and I did not face any problems. Today when I booted up my wandboard I get a lot of binder transaction "transaction failed 29189" and "binder_alloc_buf, no vma" errors and my UI keeps crashing. Is it because of some fault in the RAM? If yes, how can I test the RAM on my Wandboard?

Thanks,

Gautam.

ラベル(3)
0 件の賞賛
返信
1 返信

1,087件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gautam

please refer to ddr tester tool

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信