Big Latencies in the ethernet connection for the I.MX6 sabrelite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Big Latencies in the ethernet connection for the I.MX6 sabrelite

1,072 次查看
mohamad-ahmad
Contributor III

Hello,

I have the sabrelite board, and i am running the linux image existing here (https://boundarydevices.com/debian-8-3-jessie-for-i-mx6-boards-february-2016-kernel-3-14-28/) . The problem that is with the ethernet connection with this board i am experiencing a widely latencies and sometimes the ssh connection doesn't work and the response time is too slow.

I have found some proposed solution like this (i.MX6Q SabreSD Catastrophic Ethernet Latencies​, Implications of setting enable_wait_mode=off in 3.0.35  ) but i dont know how i can change the kernel params to set enable_wait_mode=off like is mentioned in the solutions page.

thanks for the help,

Mohamad

标签 (2)
0 项奖励
回复
2 回复数

832 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mohamad

in general kernel boot parameter enable_wait_mode=off

aslo can be used with 3.14.28 kernel, as shown for example on

U-boot.imx fails when loading zImage with iniramfs created with bitbake for custom board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

832 次查看
mohamad-ahmad
Contributor III

Hi Igor,

can i do the upgrade for u-boot directly on the sabrelite board with the linux image existing here (https://boundarydevices.com/debian-8-3-jessie-for-i-mx6-boards-february-2016-kernel-3-14-28/) .?

Best regards

Mohamad

0 项奖励
回复