Beta Version of mx8m_mx8mm_encrypted_boot.txt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beta Version of mx8m_mx8mm_encrypted_boot.txt

1,393件の閲覧回数
jim_albanese
Contributor I
Hello,
I have successfully signed and authenticated u-boot, the kernel image, the device tree blob, the entire root file system and a select portion of the root file system (used for faster boot up) on both the imx8mq-evk and the imx8mm-evk.
Unfortunately, I haven't had the same level of success with encryption.  I believe one of the issues is that the RNG is not active on the EVK so I could not create the DEK blob.  I could use help with the following item.
There are guides for HAB4 that can be found in the Yocto build.  The following three guides can be found in my build at:
/build/build/tmp/work/imx8mmevk-ips-linux/u-boot-imx/2018.03-r0/git/doc/imx/hab/habv4/guides/
* mx6_mx7_secure_boot.txt
* mx6_mx7_encrypted_boot.txt
* mx8m_mx8mm_secure_boot.txt
It would be extremely helpful if we could get the mx8m_mx8mm_encrypted_boot.txt from NXP.  I checked the latest release of these guides at : https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides?h=imx_v2019.04_4.19.3... , and did not find it.
Is there a beta version of this document available?
Thanks,
Jim
imx8 mini‌ imx8mq-evk‌ imx8mm_evk #encrypted boot#encrypted_boot
0 件の賞賛
返信
2 返答(返信)

1,293件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the document, You requested is not ready yet. Sorry.

Regards,

Yuri.

0 件の賞賛
返信

1,293件の閲覧回数
jim_albanese
Contributor I

Hi YuriMuhin_ng‌,

Thanks for the quick response.  Looking forward to the release.

Best Regards,

Jim

0 件の賞賛
返信