Behavior of i.mx6 when network device connected by pcie reboots

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Behavior of i.mx6 when network device connected by pcie reboots

1,157 次查看
heecheol_jung
Contributor II

I connect i.mx6 and network device (ex> QCT mdm chipset) by PCIe interface.

When the connected network device is rebooted, i.MX6 hangs.

The adb device can not be detected through the 'adb devices' command, and the uart console does not work either.

I think it need to reboot by kernel panic or watchdog, how do I set it?

标签 (2)
0 项奖励
回复
2 回复数

1,075 次查看
igorpadykov
NXP Employee
NXP Employee

Hi y heecheol

one can try to use wdog for rebooting, for wdog connection please check

i.MX6Q Sabre SD schematic

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
SABRE Platform for Smart Devices|NXP 

Wdog driver is described in Linux Manual included in linux documentation found on

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,075 次查看
heecheol_jung
Contributor II

Dear Igor

sorry for late response.

The hang problem was solved by kernel panic via modem-monitor. (+modify kernel config)

I have additional question about scenario when rebooting with pcie connected.

(Network device < (PCIe) > i.MX6)

 

In the above state,  is each of the reboot scenarios with modem-monitor shown below?

1. Network device reboot

> Network device reboot

> Detect PCIe disconnect in i.MX6

> i.MX6 also reboots at the same time to re-connect to PCIe

> As a result, Network device and i.MX6 reboot once

2. i.MX6 reboot

> i.MX6 reboot

> Detect PCIe disconnect in i.MX6 after reboot

> i.MX6 and Network device are reboot

> As a result, Network device reboot once and i.MX6 reboot twice

Thanks & regards

heecheol.jung

0 项奖励
回复