Bayer to rgb image correction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bayer to rgb image correction

1,670 Views
dhananajysharma
Contributor II

Hi, I am using Aptina 5Mp sensor for capturing an image attached to IMX6 wandboard.

once  demosiacing is performed on bayer data. The image has quadrant like structure means(there are four plane in the image), sometime possibly two planes.

i don't understand where is the problem?
or what extra image processing has to be done ?

do stitching is required for processing correct image?

 

Also,

I have Fish-eye lens and using following algorithm to correct lens distortion.

http://www.tannerhelland.com/4743/simple-algorithm-correcting-lens-distortion/

this is not correcting the image properly.

I have attached the code.

 

Any help will be appreciated.

Original Attachment has been moved to: demosac.cpp.zip

0 Kudos
Reply
0 Replies