Battery sizing using SNVS_LP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Battery sizing using SNVS_LP

1,044 Views
ScottKerstein
Contributor III

Document Number: AN4509 Rev. 0, 09/2012 "i.MX 6Dual/6Quad Power Consumption Measurement" App Note states "The power consumption of SNVS is comparatively negligible except in Deep Sleep Mode” and doesn’t go into any more details

“Negligible” is a fuzzy word for something that is always on when coin cell is attached (SNVS_LP.) 

There must be some current which will help to size the battery as how long the need to have backup.

Are there any characterization results?

Thanks, in advance,

Scott

Labels (1)
0 Kudos
Reply
1 Reply

955 Views
Yuri
NXP Employee
NXP Employee

Hello,

  To estimate battery options, please use “Stop Mode Current and Power Consumption” table

(SNVS Only mode) in the i.MX6 Datasheet(s), since in this mode supply current is provided by

battery.

 

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQAEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply