Basics to stream over iMX6+LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basics to stream over iMX6+LVDS

1,567 Views
rinkeshpatel
Contributor II

Hi, I am new to iMX family and we want to stream video using iMX6 Dual over LVDS.

1) Can you please suggest whatall modifications I need to do in which driver.

2) Which API of ldb.c I should call to initiate transfer over LVDS?

3) How to get frames from Frame buffer processed by IPU to stream over LVDS?

0 Kudos
5 Replies

969 Views
Yuri
NXP Employee
NXP Employee

  It may be recommended to use the Gstreamer, please refer to the

following resources :

https://community.freescale.com/docs/DOC-93387

https://community.freescale.com/thread/340677

http://boundarydevices.com/streaming-camera-using-gstreamer/


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

969 Views
rinkeshpatel
Contributor II

It is really helpful

Thank you

0 Kudos

969 Views
rinkeshpatel
Contributor II

Thank you verymuch Yuri Muhin

Rinkesh Patel

0 Kudos

969 Views
saurabh206
Senior Contributor III

Hi

Rinkesh

What do you mean by stream video using imx6 Dual over LVDS?

If want your display to be LVDS than you can modified your bootargs to "video=mxcfb0:dev=ldb,LDB-XGA,if=RGB565".

Thanks

Saurabh

0 Kudos

969 Views
rinkeshpatel
Contributor II

Yes I understood. Thank you very much

0 Kudos