Basics to stream over iMX6+LVDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Basics to stream over iMX6+LVDS

1,532件の閲覧回数
rinkeshpatel
Contributor II

Hi, I am new to iMX family and we want to stream video using iMX6 Dual over LVDS.

1) Can you please suggest whatall modifications I need to do in which driver.

2) Which API of ldb.c I should call to initiate transfer over LVDS?

3) How to get frames from Frame buffer processed by IPU to stream over LVDS?

0 件の賞賛
5 返答(返信)

934件の閲覧回数
Yuri
NXP Employee
NXP Employee

  It may be recommended to use the Gstreamer, please refer to the

following resources :

https://community.freescale.com/docs/DOC-93387

https://community.freescale.com/thread/340677

http://boundarydevices.com/streaming-camera-using-gstreamer/


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

934件の閲覧回数
rinkeshpatel
Contributor II

It is really helpful

Thank you

0 件の賞賛

934件の閲覧回数
rinkeshpatel
Contributor II

Thank you verymuch Yuri Muhin

Rinkesh Patel

0 件の賞賛

934件の閲覧回数
saurabh206
Senior Contributor III

Hi

Rinkesh

What do you mean by stream video using imx6 Dual over LVDS?

If want your display to be LVDS than you can modified your bootargs to "video=mxcfb0:dev=ldb,LDB-XGA,if=RGB565".

Thanks

Saurabh

0 件の賞賛

934件の閲覧回数
rinkeshpatel
Contributor II

Yes I understood. Thank you very much

0 件の賞賛