Ball size of i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ball size of i.MX6SL

Jump to solution
543 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about ball size of i.MX6SL.

I read a Figure 50 of following document but can't read the lower right letters.(Please see the red circle.)

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6SLCEC.pdf 

pastedImage_2.png

I think it shows in Table 64 of the document.

Could you tell me which parameter is it ?

Ko-hey

Labels (2)
0 Kudos
1 Solution
492 Views
art
NXP Employee
NXP Employee

Yes, these parameters are 'eee' (upper) and 'fff' (lower) as listed in the Table 64.


Have a great day,
Artur
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
493 Views
art
NXP Employee
NXP Employee

Yes, these parameters are 'eee' (upper) and 'fff' (lower) as listed in the Table 64.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos