BT call Audio not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BT call Audio not working

1,371件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi All,

I'm working on Android 6.0.1 BSP. wl12xx BT module i'm using. 

When i make a call Ringtone is coming on sabresd board. But after attending a call nothing on sabre board audio OUT, audio IN also not working.

Can you give me feedback on this.

Regards,

Aravinth

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,192件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Have you try, without the Bluetooth module,  the call , because the audio it is redirected, and it also happens this behavior in a nexus phone if you do not terminate the BT connection.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,192件の閲覧回数
aravinthkumarja
Senior Contributor II

Without BT connection i can able to hear sound on mobile. But i want it on board, Like BT Hfp support.

Regards,

Aravinth

0 件の賞賛
返信