BSP for uC/OS for i.MX6SX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP for uC/OS for i.MX6SX

1,200 Views
aivchenko
Contributor II

I can see that NXP has a BSP which supports i.MX6 UltraLite with uC/OS III.

Do you have BSP which can be used with uC/OS III and has support for MAC/NIC and USB so I can use uC/OS stacks for it?

Thanks,

--Alex

Labels (1)
0 Kudos
Reply
1 Reply

1,138 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alex,

The Micrium uC/OS RTOS and tools are provided and supported by Micrum so I would recommend contacting them directly for more information on the features available as part of their uC/OS-III with support for the i.MX6 processors.

Regards,

0 Kudos
Reply