BSP for uC/OS for i.MX6SX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP for uC/OS for i.MX6SX

1,262件の閲覧回数
aivchenko
Contributor II

I can see that NXP has a BSP which supports i.MX6 UltraLite with uC/OS III.

Do you have BSP which can be used with uC/OS III and has support for MAC/NIC and USB so I can use uC/OS stacks for it?

Thanks,

--Alex

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,200件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alex,

The Micrium uC/OS RTOS and tools are provided and supported by Micrum so I would recommend contacting them directly for more information on the features available as part of their uC/OS-III with support for the i.MX6 processors.

Regards,

0 件の賞賛
返信