Hi, Guys
I got some trouble when I tried to build yocto BSP L5.15.5.
It is about qt-base.bb package comiple error, have someone ever meet the same things ?
my step on ubuntu 20.04 :
$ mkdir <Yocto Project>
$ cd <Yocto Project>
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-honister -m imx- 5.15.5-1.0.0.xml
$ repo sync
$ EULA=1 MACHINE=imx8mpevk DISTRO=fsl-imx-xwayland
$ source ./imx-setup-release.sh -b buildxwayland
$ bitbake imx-image-full
error log as :
已解决! 转到解答。
Hi, @weilly_li
Please check the log file when "do_install" process failed.
(location: <your_env>/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.10.0-r0/tmp/log.do_install.xxxxx)
I had same issue because onnxruntime from "onnxruntime-imx" repository contained an unsafe repository.
This error information is listed on my "log.do_install.xxxxx" file.
In my case, the solution to this issue is "git config --global --add safe.directory <unsafe repo's directory>" command.
(This issue probably occurred recently. https://github.com/actions/checkout/issues/760 )
hi i saw you first used " fsl-yocto-8mp-5-15 " , suddenly
u changed to "imx-yocto-bsp-L5-15-5"
sometimes this issue caused by other files in yocto between two builds two folders :
i means can you totally delete all old files , and create new folder ,open new terminal , new repo sync and build it again , shld be ok.
Hi, @Zhiming_Liu
I tried clean this project and redownload it ! this is same error !!
command as :
bitbake -f -c clean qtbase
bitbake -f -c build qtbase
or
bitbake -f -c clean nativesdk-qtbase
bitbake -f -c build nativesdk-qtbase
Which one need to fix ? Thank
Hi, @Zhiming_Liu
I rebuild all yocto project , still same issue all time.
Did you build yocto bsp L 5.15.5 ? I offer u my log , please help me check it ...
Thank You
hi, @Zhiming_Liu
Thank You for help , I has build done about qtbase.
I found this Issue at VMWare , so I run "bitbake qtbase" after modify virtual RAM and CPUs . Now BSP task achice 21 %
I'll note here after anything problem , Thank You
protobuf git link is incorrect in the 2nd error line. "master" branch is not exist in protobuf repository.
Hi, @weilly_li
Please check the log file when "do_install" process failed.
(location: <your_env>/tmp/work/cortexa53-crypto-poky-linux/onnxruntime/1.10.0-r0/tmp/log.do_install.xxxxx)
I had same issue because onnxruntime from "onnxruntime-imx" repository contained an unsafe repository.
This error information is listed on my "log.do_install.xxxxx" file.
In my case, the solution to this issue is "git config --global --add safe.directory <unsafe repo's directory>" command.
(This issue probably occurred recently. https://github.com/actions/checkout/issues/760 )