BSP/Driver support for ISP of i.MX8M Plus EVK kit with image sensors P/N# OS08A20, OV2775

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP/Driver support for ISP of i.MX8M Plus EVK kit with image sensors P/N# OS08A20, OV2775

979件の閲覧回数
Zeel
Contributor II

We are developing a camera board, supporting the ISP functionality of i.MX8M Plus processor. We’re planning to integrate following image sensors from Omnivision with i.MX8M Plus EVK kit,

  1. OS08A20
  2. OV2775

So, can you confirm if these sensors are validated or tuned with i.MX8M Plus EVK kit earlier. And can you help us with the BSP/driver for the same, if available. Any other information around this would be great.

Thanks & Regards,

Zeel Shah

0 件の賞賛
3 返答(返信)

954件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

current bsp supports and verified ov2775 already, you can choose this dts file directly

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-o..."

 

862件の閲覧回数
djf1
Contributor I

how to choose this dts,mean how to apply?

0 件の賞賛

857件の閲覧回数
khang_letruong
Senior Contributor III

Hi @djf1 ,

You can stop at u-Boot prompt and change the fdtfile variable (or fdt_file depending on BSP version) :

Environment size: 5254/16380 bytes
u-boot=> setenv fdtfile imx8mp-evk-ov2775.dtb           
u-boot=> saveenv 
Saving Environment to MMC... Writing to MMC(1)... OK
u-boot=> boot


Regards,
Khang

0 件の賞賛