您好:
我下载的BSP包是完整的BSP压缩包,并非通过repo工具下载的。
开发板是imx6q的开发板 phyflex-imx6-2 : PFL-A-02-13237E0.A1/PBA-B-01 (i.MX6 Quad, 1GB RAM on one bank, 16MB NOR)
编译生成sdk时出现的错误,编译成镜像可以成功编译,但是生成sdk时出现错误。根据附件中的错误描述是
网络的问题:bitbake <image> -c populate_sdk 命令运行时,设置环境变量的网络环境为disable(即不可上网),但是
实际上运行bb*类型的脚本时却要从网络上下载文件,这就形成了矛盾,这是我从错误log上分析的结果。
具体这个问题该怎么总结还需要您指教!或者是怎么配置。
谢谢您
Original Attachment has been moved to: 18659_log.do_fetch.zip
Hi,
Here you are using the third commpany board, so I recommend you to contact the phyflex for help. The hardware and software are designed by them, so them known more about it. Hope this can help you.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------