BQ27621 integrated with IMX6 solo lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BQ27621 integrated with IMX6 solo lite

783件の閲覧回数
vinothrajm
Contributor III

Hi,

I am trying to  integrate the BQ27621 with IMX6 Solo Lite in android platform.

I get the driver for BQ27621 from below link:

linux-bq27xxx/bq27x00_battery.c at master · aneeshv/linux-bq27xxx · GitHub

And i added the driver and compile it .

When i booted the board and it works fine it shows the battery capacity, percentage etc.

But when I switch on and load the Wif modulei of the board and it goes  KERNEL PANIC .

 

I am using  both below versions. Both shows same problem.

I  attached the boot log file. Please find it . OR ANY other driver file for  BQ27621,Please suggest it. !

Original Attachment has been moved to: one.txt.zip

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

557件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Do you mean the Wifi is working fine if not load the BQ27621 driver? If it is the case, I think you may need to add some printk in the driver to see which part make the kernel panic.

0 件の賞賛
返信