Hi ,
I am using the kernel 4.14.78 and i am interfacing AR1335 based camera to IMX8M based board.
After interfacing,i got the proper streaming and everything went smooth, but not all time.
After rebooting ,some times i didn't get the streaming. while debugging it, i came to know that "BIT_ADDR_CH_ERR_INT" has been set on the CSI bridge and it was cleared only after the reboot/poweroff.
1)Please,Can someone tell, why this error set?
2)is there any work around to solve this problem?
Thanks in Advance
Malik Bathusha
Hello,
Unfortunately, I will not be able to assist you, since the camera that is supported by our BSP is the OV5640 and I do not have a way to test the camera that you are using. The problem can be due to several things, I recommend you to review the I2C signal, to see if you are not losing the communication at some point. However, I cannot guarantee you anything. I recommend you to go with NXP professional services, they will help you to solve your problem.
Professional Engineering Services :: NXP Semiconductors
I apologize for the inconveniences this could give you.
Best regards,
Diego.